This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I just updated CCS from v4.2.1 to v4.2.4. Also, updated to latest CGT, Spectrum Digital updates, etc.
I initiated the update through Help-->Software-->Find and Install
After the update was finished I couldn't build any of the existing projects. I got the following message:
"This project was created for a device-variant that is not currently recognized: TMS320C55XX.TMS320VC5515. Please install the device-variant descriptor, or migrate the project to one of the supported device-variants. "
When I tried to go into CCS Build in Project Properties I got the following message: "The currently displayed page contains invalid values".
Any idea how to solve this without a complete uninstall of CCS (I don't want to have to separately download the full image of CCS 4.2.4 or downgrade to a version that clearly has problems) ?
Thanks,
Shahar
It seems that the error message "TMS320C55XX.TMS320VC5515" shows because, for some reason, CCS 4.2.4 expects the following in ".cdtbuild" file:
<listOptionValue builtIn="false" value="DEVICE_CONFIGURATION_ID=TMS320C55XX.TMS320C5515"/>
instead of:
<listOptionValue builtIn="false" value="DEVICE_CONFIGURATION_ID=TMS320C55XX.TMS320VC5515"/>
Which worked perfectly fine in previous version.
This means you have to manually edit ".cdtbuild" file for each old project. Why CCS doesn't do any automatic conversion of projects is a mystery to me.
CCS should handle this. It looks like a bug to me. I'll file one. Thanks for reporting this.
ki
This wiki FAQ discusses the following CCS error:
"This project was created for a device-variant that is not currently recognized: TMS320C55XX.TMS320VC5515. Please install the device-variant descriptor, or migrate the project to one of the supported device-variants"
-Mark