This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How should one resolve the "duplicate conflicts" error generated by the CCS update from 4.2.4 to 4.2.5 just released?

It was strongly recommended to update to 4.2.5, so I did. But at the very end I got a message to also update the components using Update Manager, which I also did. At the very end I got a "Duplicate Conflicts" error window pop-up warning that parts of the product may become unusable:

DSP/BIOS
Version 5.41.0.06 in /C:/Program Files/Texas Instruments/ccsv4/eclipse/
Version 5.41.10.36 in /C:/Program Files/Texas Instruments/bios_5_41_10_36/eclipse/

I fumbled the mouse click and clicked "Yes". What damage is done? Can it be corrected? How?

  • Hi Steven,

    This is a known issue that has been raised in the past. It is ok to hit 'Yes' and continue.  We recognize that it is a confusing warning that can cause concern and is something we would like to clear up.

    Thanks

    ki