This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 4.2.1 Issue

Hi, I am using CCS 4.2.1 on windows XP platform. 

After creating new workplace & importing existing project file( eg. 2xPM_Sensorless_v1_1 available in control SUITE) it works fine as i was able to debug & hence FLASH memory was also getting erased.

But after closing the project & again opening the same, it is showing error at debug level  "An error was encountered when attempting to load the program". Further in details of error it is coming like " Failed to load program TMDS2MTRPFCKIT-2XPM_sensorless.out on target Texas Instrument XDS100V1 USB Emulator_0/C28xx".

Also at the same time console message was coming :-

C28xx: Flash Programmer: Missing Flash Programming Settings.
C28xx: Flash Programmer: Error erasing Flash memory.
C28xx: Flash Programmer: Missing Flash operation option. Operation cancelled.
C28xx: Trouble Writing Memory Block at 0x3f2000 on Page 0 of Length 0x371
Cannot write to target

Help me out of this issue.