Part Number: CODECOMPOSER
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Hi everyone,
I have a simple following code:
#include "device.h"
#include "driverlib.h"
void main(){
Device_init();
}
The function Device_init() is defined in "device.h", and I have included it.
Why I still receive the following error:
**** Build of configuration Debug for project Test_I2C **** "C:\\ti\\ccs1020\\ccs\\utils\\bin\\gmake" -k -j 20 all -O Building file: "../main.c" Invoking: C2000 Compiler "C:/ti/ccs1020/ccs/tools/compiler/ti-cgt-c2000_20.2.2.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla1 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu2 --include_path="C:/VietDucK19/CCS/I2c/Test_I2C" --include_path="C:/ti/c2000/C2000Ware_5_01_00_00/device_support/f2807x/common/include" --include_path="C:/ti/c2000/C2000Ware_5_01_00_00/device_support/f2807x/headers/include" --include_path="C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f2837xd/driverlib" --include_path="C:/ti/c2000/C2000Ware_5_01_00_00/driverlib/f2837xd/driverlib/inc" --include_path="C:/ti/ccs1020/ccs/tools/compiler/ti-cgt-c2000_20.2.2.LTS/include" -g --diag_warning=225 --diag_wrap=off --display_error_number --abi=coffabi --preproc_with_compile --preproc_dependency="main.d_raw" "../main.c" Finished building: "../main.c" Building target: "Test_I2C.out" Invoking: C2000 Linker "C:/ti/ccs1020/ccs/tools/compiler/ti-cgt-c2000_20.2.2.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla1 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu2 -g --diag_warning=225 --diag_wrap=off --display_error_number --abi=coffabi -z -m"Test_I2C.map" --stack_size=0x200 --warn_sections -i"C:/ti/ccs1020/ccs/tools/compiler/ti-cgt-c2000_20.2.2.LTS/lib" -i"C:/ti/ccs1020/ccs/tools/compiler/ti-cgt-c2000_20.2.2.LTS/include" --reread_libs --diag_wrap=off --display_error_number --xml_link_info="Test_I2C_linkInfo.xml" --rom_model -o "Test_I2C.out" "./main.obj" "../2837x_FLASH_lnk_cpu1.cmd" -llibc.a <Linking> undefined first referenced symbol in file --------- ---------------- _Device_init ./main.obj error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "Test_I2C.out" not built >> Compilation failure makefile:141: recipe for target 'Test_I2C.out' failed gmake[1]: *** [Test_I2C.out] Error 1 makefile:137: recipe for target 'all' failed gmake: *** [all] Error 2 **** Build Finished ****
Can someone help me, thank you in advance.