This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Running dslite.bat from the command line with "-b Erase" option to perform a mass erase, erases the microcontroller calibration data, rendering the microcontroller unusable (for any purpose requiring that calibration). This has been observed for Uniflash 8.5.0 and contrasts with Uniflash 4.6.0 which did not exhibit this behavior.
Details below are for MSP430G2955. As can be seen from the example command lines below, in this test Uniflash was being run to perform a mass erase, without loading a program.
Uniflash 4.6.0
Uniflash 8.5.0
Hello,
I assume the same exact ccxml file was used between the two versions. If this is the case then they may have been a change in the erase behavior (intentional or unintentional). I will need to follow up with the device and flash experts.
ki
I can definitely reproduce this issue. I would agree that the default behavior is to NOT erase INFOA.
I filed a big for this. Tracking link: https://sir.ext.ti.com/jira/browse/EXT_EP-11634
Thanks
ki