My company rolled out docker desktop in an enterprise environment with Enhanced Container Isolation enabled. I am trying to create a development environment container with the cl6x toolchain. From the ubuntu 23.10 base image I installed CGT 7.4.24 successfully. When trying to run the compiler though, even just for version info produces a Bad System Call.
cl6x --compiler_revision
invalid system call cl6x --compiler_revision
Additionally cl6x works fine in a non-enterprise container so I know somehow some security restrictions are blocking it. My question really comes down to, what is cl6x doing that requires these more privileged system calls? gcc runs fine as does any other software development tools I've tried. ECI is supposed to have minimal functional or performance impact to developers, yet cl6x is non-functional. Any insight you could provide would be appreciated. If I could identify the specific system call causing the issue maybe I could work with IT Security team to allow it but without knowing more I've gotten nowhere.
I have tried running the docker container with the following options with no success: docker run --security-opt seccomp=unconfined --cap-add=ALL
This is an strace of the above command:
/# strace cl6x --compiler_revisionexecve("/usr/local/bin/cl6x", ["cl6x", "--compiler_revision"], 0x7fffa9fd1358 /* 8 vars */) = 0[ Process PID=257 runs in 32 bit mode. ]uname({sysname="Linux", nodename="572b2f1a40d1", ...}) = 0brk(NULL) = 0xa2a8000brk(0xa2a8d40) = 0xa2a8d40set_thread_area({entry_number=-1, base_addr=0xa2a8840, limit=0x0fffff, seg_32bit=1, contents=0, read_exec_only=0, limit_in_pages=1, seg_not_present=0, useable=1}) = 0 (entry_number=12)readlink("/proc/self/exe", "/opt/c6000_7.4.24/bin/cl6x", 4096) = 26brk(0xa2c9d40) = 0xa2c9d40brk(0xa2ca000) = 0xa2ca000access("/etc/ld.so.nohwcap", F_OK) = -1 ENOENT (No such file or directory)rt_sigaction(SIGINT, {sa_handler=0x8052690, sa_mask=[INT], sa_flags=SA_RESTART}, {sa_handler=SIG_DFL, sa_mask=[], sa_flags=0}, 8) = 0rt_sigaction(SIGTERM, {sa_handler=0x8052690, sa_mask=[TERM], sa_flags=SA_RESTART}, {sa_handler=SIG_DFL, sa_mask=[], sa_flags=0}, 8) = 0rt_sigaction(SIGHUP, {sa_handler=0x8052690, sa_mask=[HUP], sa_flags=SA_RESTART}, {sa_handler=SIG_DFL, sa_mask=[], sa_flags=0}, 8) = 0rt_sigaction(SIGILL, {sa_handler=0x8052690, sa_mask=[ILL], sa_flags=SA_RESTART}, {sa_handler=SIG_DFL, sa_mask=[], sa_flags=0}, 8) = 0rt_sigaction(SIGABRT, {sa_handler=0x8052690, sa_mask=[ABRT], sa_flags=SA_RESTART}, {sa_handler=SIG_DFL, sa_mask=[], sa_flags=0}, 8) = 0rt_sigaction(SIGFPE, {sa_handler=0x8052690, sa_mask=[FPE], sa_flags=SA_RESTART}, {sa_handler=SIG_DFL, sa_mask=[], sa_flags=0}, 8) = 0rt_sigaction(SIGSEGV, {sa_handler=0x8052690, sa_mask=[SEGV], sa_flags=SA_RESTART}, {sa_handler=SIG_DFL, sa_mask=[], sa_flags=0}, 8) = 0rt_sigaction(SIGTRAP, {sa_handler=0x8052690, sa_mask=[TRAP], sa_flags=SA_RESTART}, {sa_handler=SIG_DFL, sa_mask=[], sa_flags=0}, 8) = 0rt_sigaction(SIGBUS, {sa_handler=0x8052690, sa_mask=[BUS], sa_flags=SA_RESTART}, {sa_handler=SIG_DFL, sa_mask=[], sa_flags=0}, 8) = 0rt_sigaction(SIGSYS, {sa_handler=0x8052690, sa_mask=[SYS], sa_flags=SA_RESTART}, {sa_handler=SIG_DFL, sa_mask=[], sa_flags=0}, 8) = 0rt_sigaction(SIGXCPU, {sa_handler=0x8052690, sa_mask=[XCPU], sa_flags=SA_RESTART}, {sa_handler=SIG_DFL, sa_mask=[], sa_flags=0}, 8) = 0rt_sigaction(SIGXFSZ, {sa_handler=0x8052690, sa_mask=[XFSZ], sa_flags=SA_RESTART}, {sa_handler=SIG_DFL, sa_mask=[], sa_flags=0}, 8) = 0fstat64(1, {st_mode=S_IFCHR|0620, st_rdev=makedev(0x88, 0), ...}) = 0mmap2(NULL, 4096, PROT_READ|PROT_WRITE, MAP_PRIVATE|MAP_ANONYMOUS, -1, 0) = 0xf7fe3000write(1, "7.4.24\n", 77.4.24) = 7exit_group(0) = ?+++ exited with 0 +++
Version 8.3.12 works ever so slightly better actually outputting its version information before failing:
/opt/ti-cgt-c6000_8.3.12/bin/cl6x --compiler_revision8.3.12❯ /opt/ti-cgt-c6000_8.3.12/bin/cl6x -versionTMS320C6x C/C++ Compiler v8.3.12Build Number 1WBIN-2LI-UASAR-TAR-C08D[1] 552 invalid system call /opt/ti-cgt-c6000_8.3.12/bin/cl6x -version