This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debug Server Scripting (DSS): loadRaw



Hi,

I'd like to use "loadRaw" in a DSS script to load a .bin in memory.

The documentation tell :

loadRaw

public void loadRaw(int nPage, long nAddress, java.lang.String sFilename, int nTypeSize, boolean bByteSwap)
throws ScriptingException
Load a raw file from the host to target memory (specified by start address, page and length). Filesize is automatically determined and the entire file is loaded *
Parameters:
nAddress - is the first address in the block.
nPage - the memory page. Use one of Memory.Page enumeration.
sFilename - specifies the name of the file that will store the target data.
nTypeSize - specifies the type size of the data. Affects how data is byte-swapped to account for differences in host and target endianess. For example: if the target is big endian (the host is always little endian) and you specify nTypeSize = 16 then the upper and lower bytes are swapped after loading the file - but before writing to target memory.
bByteSwap - Force a byte-swap of the data before writing to target memory. If Host and Target are difference endianess - this will effectively disable the automatic endianess conversion.
Throws:
ScriptingException

According to the documentation this function has no return value, but a see that "Filesize is automatically determined and the entire file is loaded".

So, is there a way to obtain the filesize as return value? or is there any other method in a DSS script to retrieve the size of the .bin file I want to load in memory?

Thanks,

Luca.