This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am running some simulations using CCSv4 and a C64x+ Megamodule cycle-accurate simulatior, little endian, as target configuration.
I had a crash of CCS when enabling the "L1D access" on Collect code coverage and exclusive profile data properties
Regards,
Maria
.
Hi Ki,
Well, on "about Code Composer studio" it says version 4.2.4.00033. And here is the test case.
Thanks. I used the same simulator and same version of CCSv4 but still do not see the error. I would suggest looking at some of the suggestions in the troubleshooting guide.
http://processors.wiki.ti.com/index.php/Troubleshooting_CCS
if those do not help, please attach a zip of the diagnostic logs mentioned below:
http://processors.wiki.ti.com/index.php/Troubleshooting_CCS#CCS_Diagnostic_Logs
Thanks
ki
Hi Ki,
I tried cleaning the workspace (I deleted the .metadata) and also try calling eclipse.exe by command line using -clean. But I got the same problem
Here I attached the target configuration file and the logs as it was described in the wiki.