Part Number: CODECOMPOSER
Tool/software:
This bug is present on both CCS THEIA v1.5.1 and CCS v20.0.0.
When `clangd` detects a problem in a header file, this problem is both highlighted inline and listed in the "Problems" section next to output. When said problem is resolved, the highlight/problem description remains in the header file even when rebuilding the project. This includes the inline highlighting, "Problems" section description, and even the file explorer red highlighting/number of problems annotation.
This problem persists between CCS application restarts, closing/opening the same workspace, deleting the build output folders and rebuilding.