Part Number: CODECOMPOSER
Tool/software:
When debugging a target over JTAG, the memory map of the target prevents reading certain regions of memory that should be accessible according to its `.gel` file.
Steps taken:
1. Connect target over JTAG to CCS v20.0.0
2. "Run" -> "Debug Project"
3. Observe
```
C28xx_CPU1:
Memory Map Initialization Complete
```
in "GEL Output"
4. Open and check "f28379d_cpu1.gel" listed in "GEL Files" to ensure "R|W|AS2" for addresses 1480, 1500
5. Check "Data" in "Memory Map" view, confirm that the above addresses are listed as "R|W|AS2"
6. Confirm these memory addresses are not readable in debug "Watch" view
Note below: From address 0x0-0x157F is marked as "R|W|AS2" in both GEL and in Memory Map view. However, on the left sidebar of Debug view, "1480" is not readable due to memory map.