Part Number: CCSTUDIO
Tool/software:
Hello, we are experiencing an issue when trying to run the same example code on a different system with Code Composer Studio (CCS) v12.8.1. The error is described below. Could anyone help me solve the issue?
<Linking>
"../28p65x_freertos_flash_lnk_cpu1.cmd", line 69: error #10099-D: program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment/blocking fails for section ".bss" size 0x25d2 page 0. Available memory ranges:
RAMLS5 size: 0x800 unused: 0x800 max hole: 0x800
error #10010: errors encountered during linking; "WIFI_PORTING.out" not built