CODECOMPOSER: CCS variable refactor-> rename function issue

Part Number: CODECOMPOSER

Tool/software:

HI 

I recently used the refactor function to make variable naming changes.

But it will work in workspace. Can I set it to work only on a single project?

TK


  • I did find these options, I wonder if there is a Rename in project option?

  • Hello,

    Please note that CCS Eclipse has been deprecated in support. Hence the amount of support we can offer will be limited.

    That said, note that if you use the Preview option, you can select which files you want to refactor. You can just select just files in the project to have the same effect.

    Thanks

    ki