CODECOMPOSER: TMS320F280x support in Theia based CCS Create New Project Wizard

Part Number: CODECOMPOSER
Other Parts Discussed in Thread: TMS320F2808, SPRC191, C2000WARE

Tool/software:

I've used CC20.1.0  to import projects created in CCS 12.8.1 that use the TMS320F2808 successfully - it's listed as a Device variant  in Properties -> general.

However, I'm struggling to use the Create new Project Wizard in CCS v20.1.0 to create a new project for a TMS320F2808. I can't seem to find the TMS320F2808 listed as a device at the very first step in the Project Wizard. None of the TMS320F280x devices seem to be listed.

How do I create a *new* Project using a F280x device using CCS 20.1.0 ?

  • Hi Steven,

    I believe the example project requires external device support found here: https://www.ti.com/tool/SPRC191

    Regards,

    Peter

  • That's good suggestion, but not the solution. I already have SPRC191 installed at the default location. It does not seem to change the availability of TMS320F2808 in the Create New Project Wizard.

    (I also note that SPRC only comes as an .exe - so would never help on macOs or Linux boxes anyway - I see the problem on macOS and Windows - not tried Linux)

  • Hi Steven,

    It seems these devices are left out of the device mappings for the new CCS 20. I'll check with our CCS team to understand if this is on their roadmap to include and what their recommendation is. For now, it would be best to continue development using LTS CCS v12

    Regards,

    Peter

  • If I create a project in CCS v12 I can import it in to CCS20.1 and it works - build debugs, even with security password settings active.

    Are you saying this is a fluke and CCS20 does not officially support the TMS320F280x parts?

  • Hi Steven,

    This is not a fluke, the CCS v20 is backwards compatible with projects created in CCS v12 application. It is just that the F280x devices are older devices which are not present in the device mappings. The newer C2000 devices are prioritized in the build testing, especially those which are currently supported by our C2000Ware SDK

    Regards,

    Peter