Tool/software:
Hi
I'm using CCS V12.
i have imported project rfEchoTx in propriety_rf from SDK 8.3.& renamed it to rrfEchoTx.
similarly I imported the same named project from SDK 6.20
when i click on a type/symbol in a source file eg 'rfc_dataEntryGeneral_t' and then press F3 i expect CCS to bring up the file & location containing its definition/declaration.
i find that this is what happens with the project from sdk 6.20 but not wth the project from sdk 8.3 (i get "could not find symbol 'rfc_dataEntryGeneral_t' in index".)
and i also note that i get this issue with the SDK symbols of the other RF_Propriety projects imported from SDK 8.3
This is (i assume) due to something in the project properties either not being set or not being included.
i have tried to compare various elements in the 2 project properties but dont see whats missing/wrong in the 8.3 ver.
Where should i direct my focus?
thanks in advance
Hi,
Thanks for your query.
Please provide more details on the above. Which SDK are you using? Is it processor SDK or MCU+SDK?
Which device are you using?
Regards,
Tushar
Hi Tushar
thanks for your prompt response.
i found a solution..But i'm NOT sure if its the WHOLE solution.
What i did was go to project properties|c/c++General|Paths and Symbols|Symbols then added symbol "DeviceFamily_CC13X2".
i noticed that that auto added it in CCS build|Arm compiler|Predefined symbols. then rebuilt the project.
What i also noticed was that if i 1st added the symbol in CCS build|Arm compiler|Predefined symbols. and then rebuilt the project - that did not work even tho it auto added the symbol to c/c++General|Paths and Symbols|Symbols.
to answer your questions: devices are cc1352 & cc1312. SDK is simplelink_cc13xx_cc26xx_sdk_8_30_01_01
i dont understand your question - "Is it processor SDK or MCU+SDK".
regards
moshe
Hi Marie
My 'solution' appears to be the answer...all is well...no errors/warnings.
cheers
moshe