This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
I try to compile a mixed C / asm project.
Using CSS v5 for the MSP430F5438A
I get a really odd error message:
[E0300] The following symbols are undefined:
The problem is: There are no symbols following. And there is no line number.
Only the filename 'ta_uart.asm'.
Can anyone help please?
Thanks
Peter
Hi Peter,
how are you combining the assembly and C code? What compiler options do you set? Are you using inline assembly?
Have you had a look at page page 55 (section 3.3.2) of the CCS Guide for the MSP? Also look at the other guide here as well.
http://www.ti.com/lit/ug/slau132f/slau132f.pdf
http://www.ti.com/lit/ug/slau131f/slau131f.pdf
These have useful information, for example :
The .cdecls directive enables programmers in mixed assembly and C/C++ environments to share C
headers containing declarations and prototypes between C and assembly code.
Best Regards,
Lisa
Peter,
Thank you, the file attached correctly. Could you also send the build output of the console view in CCS? That would help see the exact command being invoked and the error message.
I am using version 4.0.0 of the compiler (shipped with CCSv5.1.0.09000), and the error I am getting clearly shows the missing symbols:
output said:C:\Users\user\Documents\testcases\ta_5f00_uart_asm>cl430 --include_path=C:\TI\ccsv5\ccs_base\msp430\include ta_5F00_uart.asm
"ta_5F00_uart.asm", ERROR! at EOF: [E0300] The following symbols are
undefined:
TACTL
TAIV
TAR
TACCTL2
TACCTL1
TACCTL0
TACCR2
TACCR1
1 Assembly Error, No Assembly WarningsErrors in Source - Assembler Aborted
>> Compilation failure
Regards,
Rafael
Hello again,
see if this thread is a useful tip for you as well.
http://e2e.ti.com/support/microcontrollers/msp43016-bit_ultra-low_power_mcus/f/166/t/127731.aspx
Best Regards,
Lisa