Part Number: CODECOMPOSER
Other Parts Discussed in Thread: PGA970, USB2ANY
Tool/software:
I'm using CCS 12.8 to align with the answer given in a previous question PGA970: Programming a binary over SPI but am open to changing versions.
I am on Windows 11 Version 23H2 OS Build 22631.5768.
We use Windows Defender for AV, I tried to add an exception for CCS, but I'm not certain it worked. A coworker said they got this board working so I'm not certain it's the AV's fault.
I tried to run the eclipsec.exe command to print out versions but it just printed out the usage without an error message so I'm not sure.
I'm using the PGA970 EVM, unsure what the revision is, and the XDS200 debug probe.
I'm trying to run the example code provided from the secure file access, it says version 1.6.
My logs are attached 7870.log.txt
The issue is simple, I try to launch the debugger and it gets stuck at "Launching PGA970_Generic_1_6: (100%)". I tried cleaning and rebuilding the project with no errors. I am able to test the debug probe connection from the .ccxml file and it reports a success. I tried rebooting the computer and unplugging/replugging the debug probe. I tried reinstalling CCS. My coworker said he needed the USB2ANY attached to get it to work, but I've tried both with and without the USB2ANY connected with the same issue.
I asked in the pga970 forum but was directed here e2e.ti.com/.../6045366