This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm trying to migrate an old 5502 project from CCS 3.1 to CCS 5. I updated it to CCS 3.3 successfully, but when I compile in 5, I am having trouble with some of the assembly files. The following code works fine in previous versions of code composer:
; test file
; this code works fine when compiled as part of the srxx project in ccs3.1/3.3, but
; in CCS5, I get "Illegal Parallel Pair: combined number of A-Unit loads is too high
psh mmap(ST1_55)
or #0740h, mmap(ST1_55) ; enable 40 bit, data sign extension, data saturation, fractional modes
mov dbl(*AR1+), XAR3
|| mov #1, T2 ; load constant 1.0
pop mmap(ST1_55) ; restore the status word
ret
In CCS5, I get "Illegal Parallel Pair: combined number of A-Unit loads is too high". Any ideas?