Hi,
I'm having trouble getting into debug mode using the XDS510LC emulator to the TMS320F28035 on a windows 7 machine. The error I am receive is:
Error connecting to the target:
Error 0x80000200/-1041
Fatal Error during: OCS,
Device driver: Problem with the Emulation Controller.
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.
I've have found other posts detailing similar problems, but have found none with a complete resolution.
I have tried following the steps which the error message presents, to only receive the same error again. I'm assuming the drivers are installed correctly,
the device shows up in my devices manager. I also went through the steps to generate the .ccxml target configuration file, and have set it up for my emulator and
my processor. I verified that its not the processor or the emulator by going through the same set up procedure in CCSv4.2.4 on a co workers machine, and CCS connected
in debug mode just fine. So basically I'm at a loss as to why I cant connect to the processor via the debugger, so any help, or a link to a previously answered post
that I may have missed would be appreciated.
Thanks!
-Jon