This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am running CCS 5.1 with valid subscription and do not get the update on c2000 cgtools 6.1.0.
From http://processors.wiki.ti.com/index.php/Production_Compiler_Releases, it should be available since 2012-03-21.
My setup only shows cgtools 6.0.2 (Window/preferences/Code composer Studio/Build/Compilers).
The "available software sites" includes "http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/codegen/Updates/p2win32"
Where/how can I get cgtools 6.1.0?
HI Stephan,
I can see if we can get them to you, I know these tools should be on the update sites. The problem with the code generation tools download site is that only a code size limited version is posted for the C2000.
As soon as I have feedback I will let you know.
Best Regards,
Lisa
Hi Stephan,
no worries. I will send them offline. Please send a friend or conversation request to me and I will setup an offline ftp for you.
Best Regards,
Lisa
Hello Lisa,
I am working with CCvs4 on the Solar Explorer Kit. Once I run my program it shows me this warning message.
This project was created using a version of Code Generation tools that is not currently installed: 6.0.2 [C2000]. Please install the Code Generation tools of this version, or migrate the project to one of the supported versions. SolarExplorer_PVInverter_F28M35x_C28x
Could you help me with it?
Thanks,
Sofia
Hi Sofia,
I got your friend request and will send along the tools offline.
Best Regards,
Lisa