This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Converting CCS4 to CCS5



I transferred my CCS4 code to CCS5 and compiled with an error:

Buildfile generation error occurred..

Build-configuration 'Debug' does not exist in the referenced project 'csl_f28m35x_m3'. Use the 'Properties > CCS Build > Dependencies' page to select an existing build-configuration.

Build stopped..

I can't get to Properties as the Project -> Properties item is shaded and won't let me in????

Any help, please?

  • HI Pat,

    what steps did you take to migrate?  Did you import your project using Project->Import existing CCS/Eclipse Project?  What version of v4 and v5?

    Can you please provide a bit further information?  It seems CCS is looking for the Debug Configuration of the project.  This is a typical build configuration when creating a project in CCS along with the release configuration.

    Best Regards,
    Lisa

  • Hi Lisa,

    Thanks for your response.

    THis project is a variation of your HCT_Example project (by Wonsoo Kim) that contains 2 Configurations, Debug_TX and Debug_RX that key off of pre-define symbols. I need to enter the pre-define name - but can't due to this issue.

    Yes I did migrate by import from V4.2.5 to V5.1.

    Thanks,

    Pat

     

  • OK, I got there by right-click on the project in Project Explorer and then just deleted the offending project csl_f28m35x_m3 - should I have done that?

    Now I get a linker error - missing dynamic library (Emulation package 5.0.569.0) Where do I get that?

    Thanks,

    Pat

     

  • Software updates - got it.

    I'm up, thanks.

    Pat

     

  • Hi Pat,

    no worries, you managed to work through it pretty much alone.  Much respect and all the best with development.  

    We are always here if something comes up.

    Best Regards,
    Lisa