This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 5.2 OUTPUT SECTION BUILD PROBLEM



 

**** Build of configuration Debug for project test3 ****

C:\ti\ccsv5\utils\bin\gmake -k all


'Building file: ../main.c'


'Invoking: C5400 Compiler'


"C:/ti/ccsv5/tools/compiler/c5400/bin/cl500" --include_path="C:/ti/ccsv5/tools/compiler/c5400/include" --symdebug:dwarf --diag_warning=225 --display_error_number --preproc_with_compile --preproc_dependency="main.pp"  "../main.c"


'Finished building: ../main.c'


'Building target: test3.out'


'Invoking: C5400 Linker'


"C:/ti/ccsv5/tools/compiler/c5400/bin/cl500" --symdebug:dwarf --diag_warning=225 --display_error_number -z --reread_libs --warn_sections --search_path="C:/ti/ccsv5/tools/compiler/c5400/lib" --search_path="C:/ti/ccsv5/tools/compiler/c5400/include" --map_file="test3.map" --rom_model -o "test3.out"  "./main.obj" --library="libc.a"


<Linking>


warning #10247-D: creating output section ".cio" without a SECTIONS


   specification


warning #10247-D: creating output section ".const" without a SECTIONS


   specification


warning #10210-D: creating ".stack" section with default size of 0x400; use the


   -stack option to change the default size


warning #10210-D: creating ".sysmem" section with default size of 0x400; use


   the -heap option to change the default size


'Finished building target: test3.out'


' '

 

**** Build Finished ****