Hello,
I've a project which reliably crashes CCS 5.2 + TI Keystone1 Emulators win32 1.0.4.0. The project is an adapted sample which uses DMA on all 8 cores. When I click on "Terminate" while all 8 cores are processing, first the simulator crashes and aftwards CCS. (it would be really great if CCS could be made more robust in regards to Emulator/Simulator problems - usually a hanging Emulator blocks the whole user interface thread).
Is this a known bug, or should I provide the project plus a more detailed description?
- Clemens