This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We currently run a DSP course at Imperial College using Code Composer Studio (CCS) with some DSK6713 boards and I am updating the CCS4 based laboratory assignments to work with CCS5.
I am trying to get the variables in the expressions window to update values in the program whilst the program is running. I managed to get this to work in CCS4 by editing some debugger options (the real time ones), however when I look at the"real time" icons in the tool-bar in CCS5 the options are greyed out .
Can you help me sort this?
thanks
Danny
Hi Daniel,
have you tried continuous refresh? Do you have the MCSDK installed? (You can check this in Window->Preferences->Code Composer Studio->Build->RTSC->Products)
http://processors.wiki.ti.com/index.php/Multicore_System_Analyzer
Best Regards,
LIsa
the quick response is much appreciated!
The continuous refresh doesn't work
I have the following tools (but no MCSDK):
DSP/BIOS
Grace (MSP430)
Inter-processor communication
SYS/BIOS
System Analyser (UIA Target)
XDAIS
XDC tools
how do I load the MCSDK tool? Is it perhaps because I'm using the free licence that I haven't got it?
regards
Danny
Hi Danny,
you should install the MCSDK. Should be able to do this via the updat in CCS or simply download it from the TI website. Go to ti.com and search MCSDK:
http://www.ti.com/sitesearch/docs/universalsearch.tsp?searchTerm=mcsdk&linkId=1
Please give that a try and keep us informed.
BEst Regards,
Lisa
Daniel,
I am facing the same problem here. Have you found the settings that allow realtime debug mode in the meantime - if yes I would be happy to know the details. I guess the solutions proposed from LisaTI won't work since MCSDK does not support C2000 cores as far as I understand.
Thanks in advance,
Andreas
Hi Xing,
you are very lucky I managed to catch this. Could you please do the following. Could you put your question with appropriate details (target, CCS version , mcsdk installed?, what have tried?, are you in a debug session?).
It is not easy for us to track new questions when attached to old posts like this.
Thanks and we will keep an eye open for your new post.
Best Regards,
Lisa
Hi Danny,
I am also working with CCS V5, DRV8301-Rm48 Kit at technical University of Munich. So I also faced the same problem, "real time" icons in the tool-bar in CCS5 the options are greyed out and I can not realize a continuous refresh mode to graph the actual values. did you solve the problem, achived to install MCSDK ?
thanks in advance
Mete