This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS V5 Does not match the target endianness error



Hi,

I tried to writing flash memory, but I encounter error when loading UBL. target board is DM368 ipnc and CCS is Verion 5. At first, I success flash memory writing with nand flash writing program supported by ipnc SDK, but, If I try again with TI DM368 EVM nand writer program , it occured " Does not match the target endianness" error. then try again ipnc flash writing program supported by ipnc SDK, it still occured same error forever.

error messages are :

ARM9: GEL Output:
DM368 EVM ARM Startup Sequence

ARM9: GEL Output: Disable IRQ/FIQ
ARM9: GEL Output: Flush Cache
ARM9: GEL Output: Disable MMU
ARM9: GEL Output: Setup Power Modules (All on)...ARM9: GEL Output: [Done]
ARM9: GEL Output: Setup PinMux...ARM9: GEL Output: [Done]
ARM9: GEL Output: Setup PLL1...ARM9: GEL Output: [Done]
ARM9: GEL Output: Setup PLL2...ARM9: GEL Output: [Done]
ARM9: GEL Output: Setup DDR2... (340MHz)
ARM9: GEL Output: DDR2 init is done for 16-bit Interface
ARM9: GEL Output: [Done]
ARM9: GEL Output:
Startup Complete.

ARM9: GEL Output: Disable VPSS
ARM9: GEL Output: Disable IRQ/FIQ
ARM9: GEL Output: Flush Cache
ARM9: GEL Output: Disable MMU
ARM9: GEL Output: Disable EDMA events
ARM9: GEL Output:
ARM9: GEL: File: E:\workspace_test\util\flash_utils_dm36x_2.1.0\DM36x\CCS\UBL\NAND\UBL_DM36x_NAND_IPNC.out Does not match the target endianness, not loaded. Check project build options and target configuration file (ccxml).

BR,

Choi