Other Parts Discussed in Thread: CCSTUDIO
I am having a problem when I try and build/debug my project in CCSv5. The first time that I build and debug the project it works fine, but if I attempt to build/debug a second time, I get a Java Heap error as soon as the build starts. Then it gives me an internal memory error in CCSv5 and forces me to close the workspace. Once I restart CCSv5, it builds/debugs the first time, but not any subsequent attempts. It is as if the allocated memory isn't being freed up when I terminate the debug session. I have inserted a powerpoint file showing the screen shots of the error mesages, and the changes I made to eclipse.ini and ccstudio.ini to increase the memeory space. 0066.Java Heap Error.pptx