This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI:
I have some question about global/static parameter setting to ask.
We use dm648 dsp, but the problem that I can't find way to fix it.
However, I find something unusual that maybe a breakpoint.
Here's my tooling version:
Tooling Version: CCS 3.3.82.13
Integrated Development : 5.98.0.393
BIOS Version: 5.41.13.43
CGT version: 6.0.8
DSP: dm648
example:
TVP5154.c
/*******Global Variable*********/
static _TVP5154_decObj decObj[NUM_DECODERS] =
{
{0x5E, NULL, 0, {{0, 1}, {0, 2}, {0, 4}, {0, 8}}}
};
Uint8 x = 0x5e;
static Uint8 y = 0x5e;
static TVP5154_ConfParams TVP5154_default =
{
TVP5154_MODE_NTSC,
/**< NTSC operation defayult */
TVP5154_AFMT_COMPOSITE_A,
/**< Composite channel A selection default */
TRUE
/**< BT656 sync enabled */
};
/********************************/
I watch the memory when the program running.
expect reality
x 0x5E 0x0E
Y 0x5E 0x02
In the struct, the first and the last parameter are uncorrect, but the other parameter corrent
I saw the post of E2E.
Does this problem happen because the SDSCM00039997 issue?
Even I am getting feeling like it could be because of SDSCM00039997.
Did you try modifying the value programmatically again?
HI:
I have been try and error for weeks.
I thought that it is maybe a issue from hardware.
We have two custom boards, one by our(Board_A), and another one design by a different company(Board_B).
When I load the same .out to this two boards.
Board_A has the problem as I say, but the Board_B don't.
However, the design of this two board are almost the same.(reference from the EVM648 demokit circuit)
I have no idea to find where the bug, so I try to ask TI.
I don't know where the bug is. software, hardware, CGT version, CCS version... I have been tried all possible I can try.
I hope you can give some advance to fix the bug.( I come from Taiwan. it's difficult to conversation with TI)
P.S. : My English is poor. So I'm sorry that if my grammar wrong.
HI Charles,
Let me tell you that I am not the hardware guy but based on your observation,
Charles Zhang said:We have two custom boards, one by our(Board_A), and another one design by a different company(Board_B).
When I load the same .out to this two boards.
Board_A has the problem as I say, but the Board_B don't.
I am quite sure that the issue is nothing to do with software or related tools. It has to be with hardware.