This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS4, CCS3 Emulator connection Error.

Hello.

 

When I trying to connect to the JTAG with 28335.

when use CCS4 : C28xx: Error connecting to the target: Error 0x80000240/-603 Fatal Error during: Initialization, OCS, 

C28xx: Error connecting to the target: Error 0x80000200/-1047 Fatal Error during: OCS,  PTI_ERR_EMU_CLOSE Error Occured at 0x00000000

when use CCS3 : Error connecting to the target: Error 0x00000220/-1156 Error during: Execution, OCS,  Lost processor clock. Device may be operating in a low-power mode.  Do you want to bring it out of this mode?

Error connecting to the target: Error 0x00001200/-1156 Error during: OCS, Target,  Lost processor clock. Device may be operating in a low-power mode.  Do you want to bring it out of this mode?

 

I running 28335 and JTAG without problem.. until 3weeks ago.

but suddenly I can see it.

I used Spectrumdigital XDS510USB. so I changed to TDS510USB, 2weeks ago.

and I changed computer and reinstalled CCS. but I can't solved.

please, let me know, what is problem... and What is solution?

 

 

  • Hello Dong Kyu,

    There is a lot of information here but some of it is unclear:

    kim dong kyu said:
    I running 28335 and JTAG without problem.. until 3weeks ago.

    Which one is the above description for? CCSv3 or CCSv4? Or both?

    kim dong kyu said:

    C28xx: Error connecting to the target: Error 0x80000200/-1047 Fatal Error during: OCS,  PTI_ERR_EMU_CLOSE Error Occured at 0x00000000

    when use CCS3 : Error connecting to the target: Error 0x00000220/-1156 Error during: Execution, OCS,  Lost processor clock. Device may be operating in a low-power mode.  Do you want to bring it out of this mode?

    Error connecting to the target: Error 0x00001200/-1156 Error during: OCS, Target,  Lost processor clock. Device may be operating in a low-power mode.  Do you want to bring it out of this mode?

    Both errors were encountered using the same emulators?

    Both errors refer to low-power mode. Are you sure that your device did not go into low power mode ot some sleep state? Were watchdog timers disabled?

    Thanks

    ki