Other Parts Discussed in Thread: SYSBIOS
Hi,
I am working with a C6678 and I tested the OpenMP Example 1 of the CCS Studio: "Example that demonstrates using UIA with OMP". Unfortunately when I debug the programm I get weird messages in the system analyzer, but not the expected ones.
I checked other posts and tried the following:
- switched to CGT 7.4.0
- added the gel file in the target configuration
- unchecked the box in the Auto Run Options "On a program load or restart"
I attached the program and the log file.
What can I do to ghet OpenMP working together with the System Analyzer?
Kind regards,
Timon
Used configuration:
- TMS320C6678
- Windows 7
- CCS: 5.3.0.00090
- Compiler: 7.4.0
- IPC: 1.25.0.04
- MCSDK 2.01.02.05
- System Analyzer (UIA Target) 1.00.03.25