Hi,
I'm having a problem using CCS.
CCS is version 5.3.0.00090 and installed to Windows7 64bit.
When I try to configure the memory section from RTSC configuration file,
"Add button" is gray shaded so that I can't add the memory section.
Is this a bug of CCS? Is there any workaround for this?
By the way, I also installed CCSv5.3 to Windows7 32bit for check,
but the same problem appeared. It might be bug of CCSv5.3.
best regards,
g.f.