Other Parts Discussed in Thread: CCSTUDIO, CONTROLSUITE
Hi
I have CCS 5.3.0.00090 installed on win8
I am now trying to use CCS with the LaunchPad XL. When I first plugged the LPXL in the pre-loaded demo program ran perfectly.
I tried to load on the blinking LED program several times with no success.The build seems to run OK but when the debug button is pushed in CCS the progress window shows the expected operations (i.e. launching, debug, erasing sectors, loading program, loading symols, etc) and finishes without error.
But then nothing happens! The debug view is not fully loaded, the run, stop, step buttons and so on are not enabled, the disassembly remains blank showing "No debug context" and the debug session cannot be terminated except by removing the USB connection to the device!
I have used the test configuration function to test the target configuration and it reports no errors.
I have tried also with an F28027 ControlSTICK with the same issues.
Any way I can fix this or find more info on what is happening? As I say no errors are reported in the CCS GUI as far as I can see...
EDIT: CCS4.2 loads a debug session of blinkingLED to both the controlstick and LP XL correctly on the same system...though I cannot reload the demo LP XL program as CCS fails to import the project "there is no managed make file"...
EDIT: I realised the following errors are showing up when I first open CCS, dont know if these are related though...
!SESSION 2013-03-12 12:57:03.744 -----------------------------------------------
eclipse.buildId=I20120608-1200
java.version=1.6.0_13
java.vendor=Sun Microsystems Inc.
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en_IE
Framework arguments: -product com.ti.ccstudio.branding.product
Command-line arguments: -os win32 -ws win32 -arch x86 -product com.ti.ccstudio.branding.product
!ENTRY org.eclipse.ui 2 0 2013-03-12 12:57:10.360
!MESSAGE Warnings while parsing the viewer contributions from the 'org.eclipse.ui.popupMenus' extension point
!SUBENTRY 1 org.eclipse.ui 2 0 2013-03-12 12:57:10.360
!MESSAGE invalid keybinding: Cannot bind to an incomplete key sequence: plug-in='org.eclipse.cdt.debug.ui', id='AUTOGEN:::org.eclipse.cdt.debug.ui.CEditorRulerActions/org.eclipse.cdt.debug.internal.ui.actions.CBreakpointPropertiesRulerActionDelegate'
!SUBENTRY 1 org.eclipse.ui 2 0 2013-03-12 12:57:10.360
!MESSAGE invalid keybinding: Cannot bind to an incomplete key sequence: plug-in='org.eclipse.cdt.debug.ui', id='AUTOGEN:::org.eclipse.cdt.debug.ui.CEditorRulerActions/org.eclipse.cdt.debug.internal.ui.actions.EnableDisableBreakpointRulerActionDelegate'
!SUBENTRY 1 org.eclipse.ui 2 0 2013-03-12 12:57:10.360
!MESSAGE invalid keybinding: Cannot bind to an incomplete key sequence: plug-in='org.eclipse.cdt.debug.ui', id='AUTOGEN:::org.eclipse.cdt.debug.ui.CEditorRulerActions/org.eclipse.cdt.debug.ui.actions.RulerCreateBreakpointInteractiveAction'
!SUBENTRY 1 org.eclipse.ui 2 0 2013-03-12 12:57:10.360
!MESSAGE invalid keybinding: Cannot bind to an incomplete key sequence: plug-in='org.eclipse.cdt.debug.ui', id='AUTOGEN:::org.eclipse.cdt.debug.ui.AsmEditorRulerActions/org.eclipse.cdt.debug.internal.ui.actions.asm.CBreakpointPropertiesRulerActionDelegate'
!SUBENTRY 1 org.eclipse.ui 2 0 2013-03-12 12:57:10.360
!MESSAGE invalid keybinding: Cannot bind to an incomplete key sequence: plug-in='org.eclipse.cdt.debug.ui', id='AUTOGEN:::org.eclipse.cdt.debug.ui.AsmEditorRulerActions/org.eclipse.cdt.debug.internal.ui.actions.asm.EnableDisableBreakpointRulerActionDelegate'
!SUBENTRY 1 org.eclipse.ui 2 0 2013-03-12 12:57:10.360
!MESSAGE invalid keybinding: Cannot bind to an incomplete key sequence: plug-in='org.eclipse.cdt.debug.ui', id='AUTOGEN:::org.eclipse.cdt.debug.ui.AsmEditorRulerActions/org.eclipse.cdt.debug.ui.actions.asm.RulerCreateBreakpointInteractiveAction'
!SUBENTRY 1 org.eclipse.ui 2 0 2013-03-12 12:57:10.360
!MESSAGE invalid keybinding: Cannot bind to an incomplete key sequence: plug-in='org.eclipse.cdt.dsf.ui', id='AUTOGEN:::org.eclipse.cdt.dsf.debug.ui.disassemblyRulerActions/org.eclipse.debug.ui.actions.RulerAddBreakpointAction'
!SUBENTRY 1 org.eclipse.ui 2 0 2013-03-12 12:57:10.361
!MESSAGE invalid keybinding: Cannot bind to an incomplete key sequence: plug-in='org.eclipse.cdt.dsf.ui', id='org.eclipse.cdt.dsf.debug.ui.disassembly.commands.rulerToggleBreakpoint'
!ENTRY org.eclipse.ui.workbench 2 0 2013-03-12 12:57:27.437
!MESSAGE A handler conflict occurred. This may disable some commands.
!SUBENTRY 1 org.eclipse.ui.workbench 2 0 2013-03-12 12:57:27.437
!MESSAGE Conflict for 'AUTOGEN:::org.eclipse.rtsc.xdaistools.ui.actionSet/ti.xdais.qualiti':
HandlerActivation(commandId=AUTOGEN:::org.eclipse.rtsc.xdaistools.ui.actionSet/ti.xdais.qualiti,
handler=ActionDelegateHandlerProxy(null,org.eclipse.rtsc.xdctools.sg.WorkBenchDelegate),
expression=AndExpression(ActionSetExpression(org.eclipse.rtsc.xdaistools.ui.actionSet,org.eclipse.ui.internal.WorkbenchWindow@12eabae),WorkbenchWindowExpression(org.eclipse.ui.internal.WorkbenchWindow@12eabae)),sourcePriority=16640)
HandlerActivation(commandId=AUTOGEN:::org.eclipse.rtsc.xdaistools.ui.actionSet/ti.xdais.qualiti,
handler=ActionDelegateHandlerProxy(null,org.eclipse.rtsc.xdctools.sg.WorkBenchDelegate),
expression=AndExpression(ActionSetExpression(org.eclipse.rtsc.xdaistools.ui.actionSet,org.eclipse.ui.internal.WorkbenchWindow@12eabae),WorkbenchWindowExpression(org.eclipse.ui.internal.WorkbenchWindow@12eabae)),sourcePriority=16640)
!SUBENTRY 1 org.eclipse.ui.workbench 2 0 2013-03-12 12:57:27.437
!MESSAGE Conflict for 'AUTOGEN:::org.eclipse.rtsc.xdaistools.ui.actionSet/ti.xdais.wizards.genalg':
HandlerActivation(commandId=AUTOGEN:::org.eclipse.rtsc.xdaistools.ui.actionSet/ti.xdais.wizards.genalg,
handler=ActionDelegateHandlerProxy(null,org.eclipse.rtsc.xdctools.sg.WorkBenchDelegate),
expression=AndExpression(ActionSetExpression(org.eclipse.rtsc.xdaistools.ui.actionSet,org.eclipse.ui.internal.WorkbenchWindow@12eabae),WorkbenchWindowExpression(org.eclipse.ui.internal.WorkbenchWindow@12eabae)),sourcePriority=16640)
HandlerActivation(commandId=AUTOGEN:::org.eclipse.rtsc.xdaistools.ui.actionSet/ti.xdais.wizards.genalg,
handler=ActionDelegateHandlerProxy(null,org.eclipse.rtsc.xdctools.sg.WorkBenchDelegate),
expression=AndExpression(ActionSetExpression(org.eclipse.rtsc.xdaistools.ui.actionSet,org.eclipse.ui.internal.WorkbenchWindow@12eabae),WorkbenchWindowExpression(org.eclipse.ui.internal.WorkbenchWindow@12eabae)),sourcePriority=16640)