Hello,
we are working on a MSc project to implement an audio beamforming on Lyrtech's PADK. Signal processing algorithms (filter-and-sum) and electretMics+preamp are ready.
Problem: the CCS version does not seem to support Spectrum Digital's XDS510 USB JTAG Emulator. See error and screenshots. We cannot run CCS in the Emulator
The error is:
(Your Code Composer does not support the connected target. Device driver name: "C:\CCStudio_v3.1\drivers\sdgo672xUSB.dvr")
We came across a post with a similar code error hinting to CSS 3.3 "Platinum"?!
Any advice is highly appreciated.
Thank you in advance,
Luis
The system setup is:
Code Composer Studio:
CCS Version 3.3.38.2
Integrated Development 5.98.0.219
BIOS 5.31.02
Code generation Tools v6.0.8
Board revision (00.00.00)
Target silicon revision (00.00.00)
CCS Setup:
C672x XDS510USB Emulator with sdgo672xUSB.dvr
GEL file: padk_300MHz.gel
Emulator:
XDS510 USB JTAG Emulator, Rev Level: B