Other Parts Discussed in Thread: CCSTUDIO
Hi All,
I am using dsk6416 board and part of my project requires to load two arrays from the host pc to the target dsp board via RTDX. I successfully implemented the RTDX interface, but I now have problem with the available memory, I know that the default is 1K bytes.
Can you please guide me how to set up the heap size for dynamic memory allocation on the DSK6416. I am using CCSv3.1.
Cheers.