Other Parts Discussed in Thread: OMAP-L138
HI, I'm just trying to copy a project with all of its resources/settings in the Project window to a new name in that same window, but I'm having trouble doing that. I get error messages saying something about copying resources, and it seems to go into the weeds after that. With CCS4, I could do a copy -> paste -> change name, and I was done.
Here's what I'm doing now in CCS5.0.3:
Right click/copy in Project window
Right click/paste in Project window
Get a "Copy Project" window with Project name: Copy of Xproject, with a check to "Use default location"
I get a new copy named "Copy of Xproject in Project window
When I try to rename, I get a box that says "New name". I rename it to NewProject, hit OK
Now I get a box that says: "Multiple problems have occurred / java.langNullPointerException, Building workspace/Serializing CDT Project settings
To get out of it, I click "X", and although the new copy stays resident, there are errors on build.
What's the correct procedure? Does it have anything to do with copying resources or something?
Thanks, D.M.