Hi,
I want to debug both C6455DSK and C6678EVM under unbuntu Linux, but I can't get CCSv5.0.3-Linux licensed. I used a license file of CCSv4 which worked perfectly with CCSv5.0.x-windows.
The problem seemed to be the wrong HostID value read from Linux. The hostid in the license file is the MAC address of my PC 001axxxxxxxx, but the HostID of unbuntu Linux is 007F0101 which seemed to be a IP 127.0.1.1.
How can I license it?
By the way, here are some details:
The CCSv5.0.3.00028-Linux is installed on a ubuntu10.04.3 virtual machine.
The virtual machine is generated by VMware7.0 under winXP SP3.
regards,
Chengmeng