Hi,
I have a msp430 launchpad which i plan to program in code composer studio version 5.4.0.
I plan to run a "Example" project, however i have run into a problem well trying to run a example.
The example project i have picked is the project in which the board measures the temperature.
When i debug the program the code goes to the chip okay, but for some reason i don't receive any readings back. all i get in the following screenshot.
http://postimg.org/image/xuwn0t153/
"Can't find a source file at "/db/ztree/library/trees/gep/gep-e78x/src/ti/targets/msp430/rts430/boot_4.0.c"
Locate the file or edit the source lookup path to include its location."
Any ideas how to fix this issue?
Many Thanks for the help,
Franks