This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: Can't find source file

Other Parts Discussed in Thread: MSP430FR5969

I have a new project for the FRAM Wolverine MSP430FR5969.  The project compiles without errors or warnings but when I click on Debug it loads the code to the micro and immediately starts running the code instead of stopping at main so I can single step.  If I then click on Pause it complains it cannot find the source:

Can't find a source file at "/tmp/TI_MKLIBeR36VQ/SRC/copy_decompress_rle.c"
Locate the file or edit the source lookup path to include its location.

I have run to main selected.  This is a new project that I started from scratch so I probably just have something set up wrong. 

ideas welcome!

  • Hi Don,

    can you share a bit more info, possibly even the project offline (my ID is a link for a friend/conversation request).

    - what ccs version are you using

    - what are your settings

    - have you verified you are using a main

    The message you get when hitting pause is likely due to a halt in the rts library.

    Best Regards,

    Lisa

  • Don Powrie said:
    The project compiles without errors or warnings but when I click on Debug it loads the code to the micro and immediately starts running the code instead of stopping at main so I can single step.  If I then click on Pause it complains it cannot find the source

    The usual cause for that is WDT fires during C startup code