This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv5.4.0.00091 - java.lang.NullPointerException

Guru 10750 points
Other Parts Discussed in Thread: CCSTUDIO, OMAP-L138

Hi,

I installed the C6748 StarterWare (v1_20_03_03) and compiled one of the examples which worked fine, when I changed the options->CCS General->Compiler Version from "TI v7.2.1" to "TI v7.4.2" and tried to recompile the project I get the below error

"Errors occurred during the build.
Errors running builder 'CDT Builder' on project 'uart_c674x_c6748_evmC6748'.
java.lang.NullPointerException"

The project.log includes - 

"!CONFIGURATION: 'com.ti.ccstudio.buildDefinitions.C6000.Debug.1367553844' [Sun Jun 09 08:17:13 IDT 2013]

!TOOL: 'com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.compilerDebug.1842768691'

!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.CODE_STATE

!WARNING: Unresolved option: com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.LITTLE_ENDIAN"

it is the same for all the examples, I have to redefine a new project to overcome this error, what could be the issue?

Thanks,

HR

  • Sounds like they may have deprecated or removed/changed some of the build options in the newer build tools. Check your build options, especially the ones related to the warnings (ex. endianness, etc). You also may want to stick with the older version of the build tools.,

    ki

  • Hi Ki-Soo,

    I compared the compiler line and they are both the same with some place changes, the original Compiler Version is "TI v7.2.1" but it uses the existing CGT which is "TI v7.4.2"

    Thanks,

    HR

  • Did you find a work around or a fix?  I have the same issue.

  • Hi David,

    I defined a new CCS project added the files and it worked fine,

    Thanks,

    HR

  • I have the same issues, all projects imported from v5.3 cannot be built anymore, also some libraries projects says "Nothing to build". 

    All workspaces were imported then imported projects into a new workspace, but now my projects cannot be built anymore, there is a box displaying:
    "'Build Project' has encountered a problem. Errors during the build."
    The Details button says:
     
    Errors occurred during the build.
    Errors running builder 'CDT Builder' on project 'Bootloader'.
    java.lang.NullPointerException

    Creating new projects didn't help either unfortunately. Any idea? Should I revert to v5.3 so that I can continue working?

    Best regards,

    David.

  • For what it's worth.  When I import an existing CCS project into CCSv5.4 (which built in CCSv5.2) I can build.  As soon as I change "Compiler version" to TI v7.4.2 I can no longer build (i.e. NullPointerException).  After selecting the TI v7.4.2 complier there are changes to the .cproject and .ccsproject files.  If I revert these files using my source control I can build again..... until I once again select the TI v7.4.2 compiler!!

    I can successfully select the following tools and build (of course never previously selecting the TI v7.4.2 compiler):

    Compiler version: TI v7.3.12

    SYS/BIOS: 6.35.0.20

    XDCtools version: 3.24.6.63

  • Funny thing is I have another computer which was updated successfully from v5.3 to v5.4 via web installer and is using 7.4.2 without problems. On my PC the updates didn't work and then I removed CCS completely, installed from offline installer and yet doesn't work. So back to 5.3 which works with 7.3.12.

  • I decided to give one more go at v5.4 so I upgraded through Help->Check for updates menu and this time worked fine (a different thread, posted here), imported projects and they were compiled but as soon as I selected 7.4.2 compiler, I was getting that error. Reverting back didn't help, but restoring .cproject files fixed the problem and their properties show old revisions of 7.3.12 compiler, SYS/BIOS, XDC,  but in square brackets shows that they are using the newer version (7.4.2). Maybe this would be helpful for developers. 

  • David and David,

    Are you both also trying to build the C6748 starterware example? I tried with a few non-starterware sys/bios example (importing old 5.2 projects into 5.4 and use CGT 7.4.2) and there are no issues. I'm wondering if it is project specific.

    Thanks

    ki

  • No, my project is specific to our application and has a few months of development already. It is based on SYS/BIOS. Try importing from v5.3 that uses 7.3.12 if you can and change compiler to 7.4.2.

    Thanks,

    David.

  • No, I'm working with an existing project that was developed to work on LogicPD's OMAP-L138 eval board.  Would you be interested in viewing the .cproject and .ccsproject files pre and post (i.e. working and broken) compiler selection change?  Would that provide you with enough info to identify the issue?

  • David Luca said:
    Try importing from v5.3 that uses 7.3.12 if you can and change compiler to 7.4.2.

    Tried exactly this and still no issues.

    What versions of SYS/BIOS and XDC were you using in 5.3?

  • David McCreight said:
     Would you be interested in viewing the .cproject and .ccsproject files pre and post (i.e. working and broken) compiler selection change?  Would that provide you with enough info to identify the issue?

    It is worth a try. Please attach them here.

  • First time posting a file to this forum so hopefully this goes as planned.  I renamed my .cproject file to cproject.txt and .ccsproject to ccsproject.txt prior to posting.  I then change the compiler version to 7.4.2 and try to build, but receive the failure.  I renamed the two files again but appended BAD to the file names (i.e. cprojectBAD.txt and ccsprojectBAD.txt).

    <?xml version="1.0" encoding="UTF-8" standalone="no"?>
    <?ccsproject version="1.0"?>
    
    <projectOptions>
    <deviceVariant value="com.ti.ccstudio.deviceModel.C6000.GenericC674xDevice"/>
    <deviceEndianness value="little"/>
    <codegenToolVersion value="7.3.1"/>
    <isElfFormat value="false"/>
    <connection value=""/>
    <rts value="libc.a"/>
    <templateProperties value="id=org.eclipse.rtsc.project.templates.EmptyRtscApplication,buildProfile=release,isHybrid=true,"/>
    <deviceFamily value="C6000"/>
    </projectOptions>
    

    <?xml version="1.0" encoding="UTF-8" standalone="no"?>
    <?fileVersion 4.0.0?>
    
    <cproject storage_type_id="org.eclipse.cdt.core.XmlProjectDescriptionStorage">
    	<storageModule configRelations="2" moduleId="org.eclipse.cdt.core.settings">
    		<cconfiguration id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142">
    			<storageModule buildSystemId="org.eclipse.cdt.managedbuilder.core.configurationDataProvider" id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142" moduleId="org.eclipse.cdt.core.settings" name="Debug">
    				<externalSettings/>
    				<extensions>
    					<extension id="com.ti.ccstudio.binaryparser.CoffParser" point="org.eclipse.cdt.core.BinaryParser"/>
    					<extension id="com.ti.ccstudio.errorparser.CoffErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    					<extension id="com.ti.ccstudio.errorparser.LinkErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    					<extension id="com.ti.ccstudio.errorparser.AsmErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    					<extension id="org.eclipse.rtsc.xdctools.parsers.ErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    				</extensions>
    			</storageModule>
    			<storageModule moduleId="cdtBuildSystem" version="4.0.0">
    				<configuration artifactExtension="out" artifactName="dsp6840" buildProperties="" cleanCommand="${CG_CLEAN_CMD}" description="" errorParsers="org.eclipse.rtsc.xdctools.parsers.ErrorParser;com.ti.ccstudio.errorparser.CoffErrorParser;com.ti.ccstudio.errorparser.LinkErrorParser;com.ti.ccstudio.errorparser.AsmErrorParser" id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142" name="Debug" parent="com.ti.ccstudio.buildDefinitions.C6000.Debug" postbuildStep="&quot;${CCE_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin.bat&quot; &quot;${BuildArtifactFileName}&quot; &quot;${BuildArtifactFileBaseName}.bin&quot; &quot;${CG_TOOL_ROOT}/bin/ofd6x.exe&quot; &quot;${CG_TOOL_ROOT}/bin/hex6x.exe&quot; &quot;${CCE_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin.exe&quot;">
    					<folderInfo id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142." name="/" resourcePath="">
    						<toolChain id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.DebugToolchain.708327608" name="TI Build Tools" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.DebugToolchain" targetTool="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.linkerDebug.1543605365">
    							<option id="com.ti.ccstudio.buildDefinitions.core.OPT_TAGS.1899145038" superClass="com.ti.ccstudio.buildDefinitions.core.OPT_TAGS" valueType="stringList">
    								<listOptionValue builtIn="false" value="DEVICE_CONFIGURATION_ID=com.ti.ccstudio.deviceModel.C6000.GenericC674xDevice"/>
    								<listOptionValue builtIn="false" value="DEVICE_ENDIANNESS=little"/>
    								<listOptionValue builtIn="false" value="OUTPUT_FORMAT=COFF"/>
    								<listOptionValue builtIn="false" value="CCS_MBS_VERSION=5.1.0.01"/>
    								<listOptionValue builtIn="false" value="LINKER_COMMAND_FILE=OMAPL138_DSP.gel"/>
    								<listOptionValue builtIn="false" value="RUNTIME_SUPPORT_LIBRARY=libc.a"/>
    								<listOptionValue builtIn="false" value="XDC_VERSION=3.23.2.47"/>
    								<listOptionValue builtIn="false" value="RTSC_PRODUCTS=com.ti.rtsc.SYSBIOS:6.33.5.46;"/>
    								<listOptionValue builtIn="false" value="OUTPUT_TYPE=rtscApplication:executable"/>
    								<listOptionValue builtIn="false" value="RTSC_MBS_VERSION=2.2.0"/>
    							</option>
    							<option id="com.ti.ccstudio.buildDefinitions.core.OPT_CODEGEN_VERSION.954101673" name="Compiler version" superClass="com.ti.ccstudio.buildDefinitions.core.OPT_CODEGEN_VERSION" value="7.3.1" valueType="string"/>
    							<targetPlatform id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.targetPlatformDebug.1349865723" name="Platform" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.targetPlatformDebug"/>
    							<builder arguments="-k -j2" buildPath="${BuildDirectory}" id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.builderDebug.1317022926" keepEnvironmentInBuildfile="false" name="GNU Make" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.builderDebug"/>
    							<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.1491843270" name="C6000 Compiler" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug">
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.SILICON_VERSION.430795896" name="Target processor version (--silicon_version, -mv)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.SILICON_VERSION" value="6748" valueType="string"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL.1748535696" name="Debugging model" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL.SYMDEBUG__DWARF" valueType="enumerated"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEFINE.502372910" name="Pre-define NAME (--define, -D)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEFINE"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.INCLUDE_PATH.794594233" name="Add dir to #include search path (--include_path, -I)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.INCLUDE_PATH" valueType="includePath">
    									<listOptionValue builtIn="false" value="&quot;${CG_TOOL_ROOT}/include&quot;"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DISPLAY_ERROR_NUMBER.1999793588" name="Emit diagnostic identifier numbers (--display_error_number, -pden)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DISPLAY_ERROR_NUMBER" value="true" valueType="boolean"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DIAG_WARNING.620492902" name="Treat diagnostic &lt;id&gt; as warning (--diag_warning, -pdsw)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DIAG_WARNING" valueType="stringList">
    									<listOptionValue builtIn="false" value="225"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.ABI.1547316769" name="Application binary interface (coffabi, eabi) (--abi)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.ABI" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.ABI.coffabi" valueType="enumerated"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS.1867679426" name="C Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS.426924642" name="C++ Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS.1856635002" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS.911331399" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS"/>
    							</tool>
    							<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.linkerDebug.1543605365" name="C6000 Linker" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.linkerDebug">
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.OUTPUT_FILE.10523552" name="Specify output file name (--output_file, -o)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.OUTPUT_FILE" value="&quot;dsp6840.out&quot;" valueType="string"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.MAP_FILE.670969073" name="Input and output sections listed into &lt;file&gt; (--map_file, -m)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.MAP_FILE" value="&quot;dsp6840.map&quot;" valueType="string"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.LIBRARY.538630245" name="Include library file or command file as input (--library, -l)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.LIBRARY" valueType="libs">
    									<listOptionValue builtIn="false" value="&quot;rts6740.lib&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;libc.a&quot;"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.SEARCH_PATH.54522651" name="Add &lt;dir&gt; to library search path (--search_path, -i)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.SEARCH_PATH" valueType="stringList">
    									<listOptionValue builtIn="false" value="&quot;${CG_TOOL_ROOT}/lib&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;${CG_TOOL_ROOT}/include&quot;"/>
    								</option>
    							</tool>
    							<tool id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.1836012757" name="XDCtools" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool">
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.XDC_PATH.275687836" name="Package repositories (--xdcpath)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.XDC_PATH" valueType="stringList">
    									<listOptionValue builtIn="false" value="&quot;${BIOS_CG_ROOT}/packages&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;Z:\Documents\Licor\li6840DSP\dspsrc&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;${TARGET_CONTENT_BASE}&quot;"/>
    								</option>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.TARGET.231486148" name="Target (-t)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.TARGET" value="ti.targets.C674" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM.2107753497" name="Platform (-p)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM" value="L138SOM" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM_RAW.2144681854" name="Platform (-p)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM_RAW" value="L138SOM" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_PROFILE.73315632" name="Build-profile (-r)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_PROFILE" value="debug" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_CONFIGURATION_FILE.1029038086" name="Build configuration file (-b)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_CONFIGURATION_FILE" value="&quot;${PROJECT_ROOT}/L138SOM/config.bld&quot;" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.CODEGEN_TOOL_DIR.1919973269" name="Compiler tools directory (-c)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.CODEGEN_TOOL_DIR" value="&quot;${CG_TOOL_ROOT}&quot;" valueType="string"/>
    							</tool>
    						</toolChain>
    					</folderInfo>
    					<fileInfo id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142.1602869707" name="fir.c" rcbsApplicability="disable" resourcePath="CommonC6x/fir.c" toolsToInvoke="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.1491843270.480404142">
    						<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.1491843270.480404142" name="C6000 Compiler" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.1491843270">
    							<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL.1239635069" name="Debugging model" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL._none" valueType="enumerated"/>
    							<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL.86349139" name="Optimization level (--opt_level, -O)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL.3" valueType="enumerated"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS.896563114" name="C Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS.1940253090" name="C++ Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS.377039501" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS.273828401" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS"/>
    						</tool>
    					</fileInfo>
    					<fileInfo id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142.654866888" name="math.c" rcbsApplicability="disable" resourcePath="CommonC6x/math.c" toolsToInvoke="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.1491843270.1192103792">
    						<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.1491843270.1192103792" name="C6000 Compiler" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.1491843270">
    							<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL.2098530913" name="Optimization level (--opt_level, -O)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL._none" valueType="enumerated"/>
    							<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL.1703777706" name="Debugging model" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL.SYMDEBUG__DWARF" valueType="enumerated"/>
    							<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_FOR_SPACE.546261548" name="Optimize for code size (--opt_for_space, -ms)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_FOR_SPACE" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_FOR_SPACE._none" valueType="enumerated"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS.1225675872" name="C Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS.642237999" name="C++ Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS.869524053" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS.452722252" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS"/>
    						</tool>
    						<tool customBuildStep="true" id="org.eclipse.cdt.managedbuilder.ui.rcbs.655588280" name="Resource Custom Build Step">
    							<inputType id="org.eclipse.cdt.managedbuilder.ui.rcbs.inputtype.1790531172" name="Resource Custom Build Step Input Type">
    								<additionalInput kind="additionalinputdependency" paths=""/>
    							</inputType>
    							<outputType id="org.eclipse.cdt.managedbuilder.ui.rcbs.outputtype.2116208278" name="Resource Custom Build Step Output Type"/>
    						</tool>
    					</fileInfo>
    					<fileInfo id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142.Common6800/eventLog.c" name="eventLog.c" rcbsApplicability="disable" resourcePath="Common6800/eventLog.c" toolsToInvoke="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.1491843270.213613730">
    						<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.1491843270.213613730" name="C6000 Compiler" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.1491843270">
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS.1729046149" name="C Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS.383089800" name="C++ Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS.302446412" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS.1860314574" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS"/>
    						</tool>
    					</fileInfo>
    					<sourceEntries>
    						<entry excluding="L138SOM/package/build.cfg" flags="VALUE_WORKSPACE_PATH|RESOLVED" kind="sourcePath" name=""/>
    					</sourceEntries>
    				</configuration>
    			</storageModule>
    			<storageModule moduleId="org.eclipse.cdt.core.externalSettings"/>
    		</cconfiguration>
    		<cconfiguration id="com.ti.ccstudio.buildDefinitions.C6000.Release.1799793832">
    			<storageModule buildSystemId="org.eclipse.cdt.managedbuilder.core.configurationDataProvider" id="com.ti.ccstudio.buildDefinitions.C6000.Release.1799793832" moduleId="org.eclipse.cdt.core.settings" name="Release">
    				<externalSettings/>
    				<extensions>
    					<extension id="com.ti.ccstudio.binaryparser.CoffParser" point="org.eclipse.cdt.core.BinaryParser"/>
    					<extension id="com.ti.ccstudio.errorparser.CoffErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    					<extension id="com.ti.ccstudio.errorparser.LinkErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    					<extension id="com.ti.ccstudio.errorparser.AsmErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    					<extension id="org.eclipse.rtsc.xdctools.parsers.ErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    				</extensions>
    			</storageModule>
    			<storageModule moduleId="cdtBuildSystem" version="4.0.0">
    				<configuration artifactExtension="out" artifactName="${ProjName}" buildProperties="" cleanCommand="${CG_CLEAN_CMD}" description="" errorParsers="org.eclipse.rtsc.xdctools.parsers.ErrorParser;com.ti.ccstudio.errorparser.CoffErrorParser;com.ti.ccstudio.errorparser.LinkErrorParser;com.ti.ccstudio.errorparser.AsmErrorParser" id="com.ti.ccstudio.buildDefinitions.C6000.Release.1799793832" name="Release" parent="com.ti.ccstudio.buildDefinitions.C6000.Release" postbuildStep="&quot;${CCE_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin.bat&quot; &quot;${BuildArtifactFileName}&quot; &quot;${BuildArtifactFileBaseName}.bin&quot; &quot;${CG_TOOL_ROOT}/bin/ofd6x.exe&quot; &quot;${CG_TOOL_ROOT}/bin/hex6x.exe&quot; &quot;${CCE_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin.exe&quot;">
    					<folderInfo id="com.ti.ccstudio.buildDefinitions.C6000.Release.1799793832." name="/" resourcePath="">
    						<toolChain id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.ReleaseToolchain.1154829311" name="TI Build Tools" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.ReleaseToolchain" targetTool="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.linkerRelease.200423611">
    							<option id="com.ti.ccstudio.buildDefinitions.core.OPT_TAGS.1601292405" superClass="com.ti.ccstudio.buildDefinitions.core.OPT_TAGS" valueType="stringList">
    								<listOptionValue builtIn="false" value="DEVICE_CONFIGURATION_ID=com.ti.ccstudio.deviceModel.C6000.GenericC674xDevice"/>
    								<listOptionValue builtIn="false" value="DEVICE_ENDIANNESS=little"/>
    								<listOptionValue builtIn="false" value="OUTPUT_FORMAT=COFF"/>
    								<listOptionValue builtIn="false" value="CCS_MBS_VERSION=5.1.0.01"/>
    								<listOptionValue builtIn="false" value="RUNTIME_SUPPORT_LIBRARY=libc.a"/>
    								<listOptionValue builtIn="false" value="XDC_VERSION=3.23.2.47"/>
    								<listOptionValue builtIn="false" value="RTSC_PRODUCTS=com.ti.biospsp:3.0.1.00;com.ti.rtsc.SYSBIOS:6.33.4.39;"/>
    								<listOptionValue builtIn="false" value="LINK_ORDER="/>
    								<listOptionValue builtIn="false" value="OUTPUT_TYPE=rtscApplication:executable"/>
    								<listOptionValue builtIn="false" value="RTSC_MBS_VERSION=2.2.0"/>
    							</option>
    							<option id="com.ti.ccstudio.buildDefinitions.core.OPT_CODEGEN_VERSION.2072441558" name="Compiler version" superClass="com.ti.ccstudio.buildDefinitions.core.OPT_CODEGEN_VERSION" value="7.3.1" valueType="string"/>
    							<targetPlatform id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.targetPlatformRelease.119193846" name="Platform" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.targetPlatformRelease"/>
    							<builder arguments="-k -j2" buildPath="${BuildDirectory}" command="${CCS_UTILS_DIR}/bin/gmake" id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.builderRelease.1960294981" keepEnvironmentInBuildfile="false" name="GNU Make" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.builderRelease"/>
    							<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerRelease.1122312953" name="C6000 Compiler" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerRelease">
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.SILICON_VERSION.416193255" name="Target processor version (--silicon_version, -mv)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.SILICON_VERSION" value="6748" valueType="string"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEFINE.578831485" name="Pre-define NAME (--define, -D)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEFINE" valueType="definedSymbols">
    									<listOptionValue builtIn="false" value="C674x"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.INCLUDE_PATH.936367591" name="Add dir to #include search path (--include_path, -I)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.INCLUDE_PATH" valueType="includePath">
    									<listOptionValue builtIn="false" value="&quot;${CG_TOOL_ROOT}/include&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;${BIOSPSP_INSTALL_DIR}&quot;"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DISPLAY_ERROR_NUMBER.1297224383" name="Emit diagnostic identifier numbers (--display_error_number, -pden)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DISPLAY_ERROR_NUMBER" value="true" valueType="boolean"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DIAG_WARNING.507481834" name="Treat diagnostic &lt;id&gt; as warning (--diag_warning, -pdsw)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DIAG_WARNING" valueType="stringList">
    									<listOptionValue builtIn="false" value="225"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.ABI.671714498" name="Application binary interface (coffabi, eabi) (--abi)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.ABI" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.ABI.coffabi" valueType="enumerated"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS.2004029078" name="C Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS.1883127587" name="C++ Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS.1262924939" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS.928326112" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS"/>
    							</tool>
    							<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.linkerRelease.200423611" name="C6000 Linker" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.linkerRelease">
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.OUTPUT_FILE.798875579" name="Specify output file name (--output_file, -o)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.OUTPUT_FILE" value="&quot;${ProjName}.out&quot;" valueType="string"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.MAP_FILE.658950961" name="Input and output sections listed into &lt;file&gt; (--map_file, -m)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.MAP_FILE" value="&quot;${ProjName}.map&quot;" valueType="string"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.SEARCH_PATH.340263356" name="Add &lt;dir&gt; to library search path (--search_path, -i)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.SEARCH_PATH" valueType="stringList">
    									<listOptionValue builtIn="false" value="&quot;${CG_TOOL_ROOT}/lib&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;${CG_TOOL_ROOT}/include&quot;"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.LIBRARY.444212762" name="Include library file or command file as input (--library, -l)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.LIBRARY" valueType="libs">
    									<listOptionValue builtIn="false" value="&quot;libc.a&quot;"/>
    								</option>
    							</tool>
    							<tool id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.226238413" name="XDCtools" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool">
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.XDC_PATH.44416606" name="Package repositories (--xdcpath)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.XDC_PATH" valueType="stringList">
    									<listOptionValue builtIn="false" value="&quot;${BIOS_CG_ROOT}/packages&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;${BIOSPSP_INSTALL_DIR}/drivers&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;C:\Licor\li6840DSP\dspsrc&quot;"/>
    									<listOptionValue builtIn="false" value="${TARGET_CONTENT_BASE}"/>
    								</option>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.TARGET.359508193" name="Target (-t)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.TARGET" value="ti.targets.C674" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM.1703141961" name="Platform (-p)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM" value="L138SOM" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM_RAW.1257005979" name="Platform (-p)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM_RAW" value="L138SOM" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_PROFILE.1109575038" name="Build-profile (-r)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_PROFILE" value="release" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_CONFIGURATION_FILE.1173860905" name="Build configuration file (-b)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_CONFIGURATION_FILE" value="&quot;${PROJECT_ROOT}/L138SOM/config.bld&quot;" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.CODEGEN_TOOL_DIR.1831695366" name="Compiler tools directory (-c)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.CODEGEN_TOOL_DIR" value="&quot;${CG_TOOL_ROOT}&quot;" valueType="string"/>
    							</tool>
    						</toolChain>
    					</folderInfo>
    					<fileInfo id="com.ti.ccstudio.buildDefinitions.C6000.Release.1799793832.OMAPL138_DSP.gel" name="OMAPL138_DSP.gel" rcbsApplicability="disable" resourcePath="OMAPL138_DSP.gel" toolsToInvoke=""/>
    					<sourceEntries>
    						<entry excluding="OMAPL138_DSP.gel|L138SOM/package/build.cfg" flags="VALUE_WORKSPACE_PATH|RESOLVED" kind="sourcePath" name=""/>
    					</sourceEntries>
    				</configuration>
    			</storageModule>
    			<storageModule moduleId="org.eclipse.cdt.core.externalSettings"/>
    		</cconfiguration>
    	</storageModule>
    	<storageModule moduleId="cdtBuildSystem" version="4.0.0">
    		<project id="li6840.com.ti.ccstudio.buildDefinitions.C6000.ProjectType.266474454" name="C6000" projectType="com.ti.ccstudio.buildDefinitions.C6000.ProjectType"/>
    	</storageModule>
    	<storageModule moduleId="refreshScope" versionNumber="1">
    		<resource resourceType="PROJECT" workspacePath="/li6840"/>
    	</storageModule>
    	<storageModule moduleId="org.eclipse.cdt.core.language.mapping">
    		<project-mappings>
    			<content-type-mapping configuration="" content-type="org.eclipse.cdt.core.asmSource" language="com.ti.ccstudio.core.TIASMLanguage"/>
    			<content-type-mapping configuration="" content-type="org.eclipse.cdt.core.cHeader" language="com.ti.ccstudio.core.TIGCCLanguage"/>
    			<content-type-mapping configuration="" content-type="org.eclipse.cdt.core.cSource" language="com.ti.ccstudio.core.TIGCCLanguage"/>
    			<content-type-mapping configuration="" content-type="org.eclipse.cdt.core.cxxHeader" language="com.ti.ccstudio.core.TIGPPLanguage"/>
    			<content-type-mapping configuration="" content-type="org.eclipse.cdt.core.cxxSource" language="com.ti.ccstudio.core.TIGPPLanguage"/>
    		</project-mappings>
    	</storageModule>
    	<storageModule moduleId="org.eclipse.cdt.internal.ui.text.commentOwnerProjectMappings"/>
    	<storageModule moduleId="scannerConfiguration"/>
    </cproject>
    

    <?xml version="1.0" encoding="UTF-8" ?>
    <?ccsproject version="1.0"?>
    <projectOptions>
    	<deviceVariant value="com.ti.ccstudio.deviceModel.C6000.GenericC674xDevice"/>
    	<deviceEndianness value="little"/>
    	<codegenToolVersion value="7.3.1"/>
    	<isElfFormat value="false"/>
    	<connection value=""/>
    	<rts value="libc.a"/>
    	<templateProperties value="id=org.eclipse.rtsc.project.templates.EmptyRtscApplication,buildProfile=release,isHybrid=true,"/>
    	<deviceFamily value="C6000"/>
    	<isTargetManual value="false"/>
    </projectOptions>
    

    <?xml version="1.0" encoding="UTF-8" standalone="no"?>
    <?fileVersion 4.0.0?>
    
    <cproject storage_type_id="org.eclipse.cdt.core.XmlProjectDescriptionStorage">
    	<storageModule configRelations="2" moduleId="org.eclipse.cdt.core.settings">
    		<cconfiguration id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142">
    			<storageModule buildSystemId="org.eclipse.cdt.managedbuilder.core.configurationDataProvider" id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142" moduleId="org.eclipse.cdt.core.settings" name="Debug">
    				<externalSettings/>
    				<extensions>
    					<extension id="com.ti.ccstudio.binaryparser.CoffParser" point="org.eclipse.cdt.core.BinaryParser"/>
    					<extension id="com.ti.ccstudio.errorparser.CoffErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    					<extension id="com.ti.ccstudio.errorparser.LinkErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    					<extension id="com.ti.ccstudio.errorparser.AsmErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    					<extension id="org.eclipse.rtsc.xdctools.parsers.ErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    				</extensions>
    			</storageModule>
    			<storageModule moduleId="cdtBuildSystem" version="4.0.0">
    				<configuration artifactExtension="out" artifactName="dsp6840" buildProperties="" cleanCommand="${CG_CLEAN_CMD}" description="" errorParsers="org.eclipse.rtsc.xdctools.parsers.ErrorParser;com.ti.ccstudio.errorparser.CoffErrorParser;com.ti.ccstudio.errorparser.LinkErrorParser;com.ti.ccstudio.errorparser.AsmErrorParser" id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142" name="Debug" parent="com.ti.ccstudio.buildDefinitions.C6000.Debug" postbuildStep="&quot;${CCE_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin.bat&quot; &quot;${BuildArtifactFileName}&quot; &quot;${BuildArtifactFileBaseName}.bin&quot; &quot;${CG_TOOL_ROOT}/bin/ofd6x.exe&quot; &quot;${CG_TOOL_ROOT}/bin/hex6x.exe&quot; &quot;${CCE_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin.exe&quot;">
    					<folderInfo id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142." name="/" resourcePath="">
    						<toolChain id="com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.DebugToolchain.630048461" name="TI Build Tools" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.DebugToolchain" targetTool="com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.linkerDebug.350983676">
    							<option id="com.ti.ccstudio.buildDefinitions.core.OPT_TAGS.348495919" superClass="com.ti.ccstudio.buildDefinitions.core.OPT_TAGS" valueType="stringList">
    								<listOptionValue builtIn="false" value="DEVICE_CONFIGURATION_ID=com.ti.ccstudio.deviceModel.C6000.GenericC674xDevice"/>
    								<listOptionValue builtIn="false" value="DEVICE_ENDIANNESS=little"/>
    								<listOptionValue builtIn="false" value="OUTPUT_FORMAT=COFF"/>
    								<listOptionValue builtIn="false" value="CCS_MBS_VERSION=5.1.0.01"/>
    								<listOptionValue builtIn="false" value="LINKER_COMMAND_FILE=OMAPL138_DSP.gel"/>
    								<listOptionValue builtIn="false" value="RUNTIME_SUPPORT_LIBRARY=libc.a"/>
    								<listOptionValue builtIn="false" value="RTSC_MBS_VERSION=2.2.0"/>
    								<listOptionValue builtIn="false" value="XDC_VERSION=3.23.2.47"/>
    								<listOptionValue builtIn="false" value="RTSC_PRODUCTS=com.ti.rtsc.SYSBIOS:6.33.5.46;"/>
    								<listOptionValue builtIn="false" value="INACTIVE_REPOS="/>
    								<listOptionValue builtIn="false" value="OUTPUT_TYPE=rtscApplication:executable"/>
    							</option>
    							<option id="com.ti.ccstudio.buildDefinitions.core.OPT_CODEGEN_VERSION.1021093644" superClass="com.ti.ccstudio.buildDefinitions.core.OPT_CODEGEN_VERSION" value="7.4.2" valueType="string"/>
    							<targetPlatform id="com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.targetPlatformDebug.1009624518" name="Platform" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.targetPlatformDebug"/>
    							<builder arguments="-k -j2" buildPath="${BuildDirectory}" id="com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.builderDebug.1278898889" name="GNU Make.Debug" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.builderDebug"/>
    							<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.compilerDebug.1352683281" name="C6000 Compiler" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.compilerDebug">
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.SILICON_VERSION.2067812913" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.SILICON_VERSION" value="6748" valueType="string"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.DEBUGGING_MODEL.866572630" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.DEBUGGING_MODEL" value="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.DEBUGGING_MODEL.SYMDEBUG__DWARF" valueType="enumerated"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.INCLUDE_PATH.668343849" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.INCLUDE_PATH" valueType="includePath">
    									<listOptionValue builtIn="false" value="&quot;${CG_TOOL_ROOT}/include&quot;"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.DISPLAY_ERROR_NUMBER.390037831" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.DISPLAY_ERROR_NUMBER" value="true" valueType="boolean"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.DIAG_WARNING.1625889665" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.DIAG_WARNING" valueType="stringList">
    									<listOptionValue builtIn="false" value="225"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.ABI.640804902" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.ABI" value="com.ti.ccstudio.buildDefinitions.C6000_7.4.compilerID.ABI.coffabi" valueType="enumerated"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.4.compiler.inputType__C_SRCS.1711597434" name="C Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.compiler.inputType__C_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.4.compiler.inputType__CPP_SRCS.1959840825" name="C++ Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.compiler.inputType__CPP_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.4.compiler.inputType__ASM_SRCS.562025301" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.compiler.inputType__ASM_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.4.compiler.inputType__ASM2_SRCS.1030348774" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.compiler.inputType__ASM2_SRCS"/>
    							</tool>
    							<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.linkerDebug.350983676" name="C6000 Linker" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.exe.linkerDebug">
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.4.linkerID.OUTPUT_FILE.1687470209" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.linkerID.OUTPUT_FILE" value="&quot;dsp6840.out&quot;" valueType="string"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.4.linkerID.MAP_FILE.1866275503" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.linkerID.MAP_FILE" value="&quot;dsp6840.map&quot;" valueType="string"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.4.linkerID.LIBRARY.1984729595" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.linkerID.LIBRARY" valueType="libs">
    									<listOptionValue builtIn="false" value="&quot;rts6740.lib&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;libc.a&quot;"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.4.linkerID.SEARCH_PATH.490768665" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.linkerID.SEARCH_PATH" valueType="libPaths">
    									<listOptionValue builtIn="false" value="&quot;${CG_TOOL_ROOT}/lib&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;${CG_TOOL_ROOT}/include&quot;"/>
    								</option>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.4.exeLinker.inputType__CMD_SRCS.7638599" name="Linker Command Files" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.exeLinker.inputType__CMD_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.4.exeLinker.inputType__CMD2_SRCS.1676742499" name="Linker Command Files" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.exeLinker.inputType__CMD2_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.4.exeLinker.inputType__GEN_CMDS.2065730672" name="Generated Linker Command Files" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.4.exeLinker.inputType__GEN_CMDS"/>
    							</tool>
    							<tool id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.814364678" name="XDCtools" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool">
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.XDC_PATH.1383473345" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.XDC_PATH" valueType="stringList">
    									<listOptionValue builtIn="false" value="${BIOS_CG_ROOT}/packages"/>
    									<listOptionValue builtIn="false" value="Z:\Documents\Licor\li6840DSP\dspsrc"/>
    									<listOptionValue builtIn="false" value="${TARGET_CONTENT_BASE}"/>
    								</option>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.TARGET.664400742" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.TARGET" value="ti.targets.C674" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM.1601042181" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM" value="L138SOM" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM_RAW.709845804" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM_RAW" value="L138SOM" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_PROFILE.1132881760" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_PROFILE" value="debug" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_CONFIGURATION_FILE.1255862715" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_CONFIGURATION_FILE" value="&quot;${PROJECT_ROOT}/L138SOM/config.bld&quot;" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.CODEGEN_TOOL_DIR.1807616128" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.CODEGEN_TOOL_DIR" value="&quot;${CG_TOOL_ROOT}&quot;" valueType="string"/>
    							</tool>
    						</toolChain>
    					</folderInfo>
    					<fileInfo id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142.CommonC6x/fir.c" name="fir.c" rcbsApplicability="disable" resourcePath="CommonC6x/fir.c" toolsToInvoke="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.1531260021">
    						<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.1531260021" name="C6000 Compiler">
    							<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL.1131464742" name="Debugging model" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL._none" valueType="enumerated"/>
    							<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL.1732027606" name="Optimization level (--opt_level, -O)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL.3" valueType="enumerated"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS.741133881" name="C Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS.659696717" name="C++ Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS.867113063" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS.588863998" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS"/>
    						</tool>
    					</fileInfo>
    					<fileInfo id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142.CommonC6x/math.c" name="math.c" rcbsApplicability="disable" resourcePath="CommonC6x/math.c" toolsToInvoke="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.681956491">
    						<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.681956491" name="C6000 Compiler">
    							<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL.1040327696" name="Optimization level (--opt_level, -O)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_LEVEL._none" valueType="enumerated"/>
    							<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL.720034030" name="Debugging model" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEBUGGING_MODEL.SYMDEBUG__DWARF" valueType="enumerated"/>
    							<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_FOR_SPACE.42438049" name="Optimize for code size (--opt_for_space, -ms)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_FOR_SPACE" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.OPT_FOR_SPACE._none" valueType="enumerated"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS.950108946" name="C Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS.1109148992" name="C++ Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS.1449493146" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS.664073275" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS"/>
    						</tool>
    						<tool customBuildStep="true" id="org.eclipse.cdt.managedbuilder.ui.rcbs.655588280.1906058083.1748459652" name="Resource Custom Build Step">
    							<inputType id="org.eclipse.cdt.managedbuilder.ui.rcbs.inputtype.1790531172.796448518.708952126" name="Resource Custom Build Step Input Type">
    								<additionalInput kind="additionalinputdependency" paths=""/>
    							</inputType>
    							<outputType id="org.eclipse.cdt.managedbuilder.ui.rcbs.outputtype.2116208278.1125195280.1570522477" name="Resource Custom Build Step Output Type"/>
    						</tool>
    					</fileInfo>
    					<fileInfo id="com.ti.ccstudio.buildDefinitions.C6000.Debug.1206718142.Common6800/eventLog.c" name="eventLog.c" rcbsApplicability="disable" resourcePath="Common6800/eventLog.c" toolsToInvoke="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.62509546">
    						<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerDebug.62509546" name="C6000 Compiler">
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS.1929547916" name="C Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS.169377621" name="C++ Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS.132132403" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS"/>
    							<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS.530873073" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS"/>
    						</tool>
    					</fileInfo>
    					<sourceEntries>
    						<entry excluding="L138SOM/package/build.cfg" flags="VALUE_WORKSPACE_PATH|RESOLVED" kind="sourcePath" name=""/>
    					</sourceEntries>
    				</configuration>
    			</storageModule>
    			<storageModule moduleId="org.eclipse.cdt.core.externalSettings"/>
    		</cconfiguration>
    		<cconfiguration id="com.ti.ccstudio.buildDefinitions.C6000.Release.1799793832">
    			<storageModule buildSystemId="org.eclipse.cdt.managedbuilder.core.configurationDataProvider" id="com.ti.ccstudio.buildDefinitions.C6000.Release.1799793832" moduleId="org.eclipse.cdt.core.settings" name="Release">
    				<externalSettings/>
    				<extensions>
    					<extension id="com.ti.ccstudio.binaryparser.CoffParser" point="org.eclipse.cdt.core.BinaryParser"/>
    					<extension id="com.ti.ccstudio.errorparser.CoffErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    					<extension id="com.ti.ccstudio.errorparser.LinkErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    					<extension id="com.ti.ccstudio.errorparser.AsmErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    					<extension id="org.eclipse.rtsc.xdctools.parsers.ErrorParser" point="org.eclipse.cdt.core.ErrorParser"/>
    				</extensions>
    			</storageModule>
    			<storageModule moduleId="cdtBuildSystem" version="4.0.0">
    				<configuration artifactExtension="out" artifactName="${ProjName}" buildProperties="" cleanCommand="${CG_CLEAN_CMD}" description="" errorParsers="org.eclipse.rtsc.xdctools.parsers.ErrorParser;com.ti.ccstudio.errorparser.CoffErrorParser;com.ti.ccstudio.errorparser.LinkErrorParser;com.ti.ccstudio.errorparser.AsmErrorParser" id="com.ti.ccstudio.buildDefinitions.C6000.Release.1799793832" name="Release" parent="com.ti.ccstudio.buildDefinitions.C6000.Release" postbuildStep="&quot;${CCE_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin.bat&quot; &quot;${BuildArtifactFileName}&quot; &quot;${BuildArtifactFileBaseName}.bin&quot; &quot;${CG_TOOL_ROOT}/bin/ofd6x.exe&quot; &quot;${CG_TOOL_ROOT}/bin/hex6x.exe&quot; &quot;${CCE_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin.exe&quot;">
    					<folderInfo id="com.ti.ccstudio.buildDefinitions.C6000.Release.1799793832." name="/" resourcePath="">
    						<toolChain id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.ReleaseToolchain.1154829311" name="TI Build Tools" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.ReleaseToolchain" targetTool="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.linkerRelease.200423611">
    							<option id="com.ti.ccstudio.buildDefinitions.core.OPT_TAGS.1601292405" superClass="com.ti.ccstudio.buildDefinitions.core.OPT_TAGS" valueType="stringList">
    								<listOptionValue builtIn="false" value="DEVICE_CONFIGURATION_ID=com.ti.ccstudio.deviceModel.C6000.GenericC674xDevice"/>
    								<listOptionValue builtIn="false" value="DEVICE_ENDIANNESS=little"/>
    								<listOptionValue builtIn="false" value="OUTPUT_FORMAT=COFF"/>
    								<listOptionValue builtIn="false" value="CCS_MBS_VERSION=5.1.0.01"/>
    								<listOptionValue builtIn="false" value="RUNTIME_SUPPORT_LIBRARY=libc.a"/>
    								<listOptionValue builtIn="false" value="XDC_VERSION=3.23.2.47"/>
    								<listOptionValue builtIn="false" value="RTSC_PRODUCTS=com.ti.biospsp:3.0.1.00;com.ti.rtsc.SYSBIOS:6.33.4.39;"/>
    								<listOptionValue builtIn="false" value="LINK_ORDER="/>
    								<listOptionValue builtIn="false" value="OUTPUT_TYPE=rtscApplication:executable"/>
    								<listOptionValue builtIn="false" value="RTSC_MBS_VERSION=2.2.0"/>
    							</option>
    							<option id="com.ti.ccstudio.buildDefinitions.core.OPT_CODEGEN_VERSION.2072441558" name="Compiler version" superClass="com.ti.ccstudio.buildDefinitions.core.OPT_CODEGEN_VERSION" value="7.3.1" valueType="string"/>
    							<targetPlatform id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.targetPlatformRelease.119193846" name="Platform" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.targetPlatformRelease"/>
    							<builder arguments="-k -j2" buildPath="${BuildDirectory}" command="${CCS_UTILS_DIR}/bin/gmake" id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.builderRelease.1960294981" keepEnvironmentInBuildfile="false" name="GNU Make" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.builderRelease"/>
    							<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerRelease.1122312953" name="C6000 Compiler" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.compilerRelease">
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.SILICON_VERSION.416193255" name="Target processor version (--silicon_version, -mv)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.SILICON_VERSION" value="6748" valueType="string"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEFINE.578831485" name="Pre-define NAME (--define, -D)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DEFINE" valueType="definedSymbols">
    									<listOptionValue builtIn="false" value="C674x"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.INCLUDE_PATH.936367591" name="Add dir to #include search path (--include_path, -I)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.INCLUDE_PATH" valueType="includePath">
    									<listOptionValue builtIn="false" value="&quot;${CG_TOOL_ROOT}/include&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;${BIOSPSP_INSTALL_DIR}&quot;"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DISPLAY_ERROR_NUMBER.1297224383" name="Emit diagnostic identifier numbers (--display_error_number, -pden)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DISPLAY_ERROR_NUMBER" value="true" valueType="boolean"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DIAG_WARNING.507481834" name="Treat diagnostic &lt;id&gt; as warning (--diag_warning, -pdsw)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.DIAG_WARNING" valueType="stringList">
    									<listOptionValue builtIn="false" value="225"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.ABI.671714498" name="Application binary interface (coffabi, eabi) [See 'General' page to edit] (--abi)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.ABI" value="com.ti.ccstudio.buildDefinitions.C6000_7.3.compilerID.ABI.coffabi" valueType="enumerated"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS.2004029078" name="C Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__C_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS.1883127587" name="C++ Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__CPP_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS.1262924939" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS.928326112" name="Assembly Sources" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.compiler.inputType__ASM2_SRCS"/>
    							</tool>
    							<tool id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.linkerRelease.200423611" name="C6000 Linker" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exe.linkerRelease">
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.OUTPUT_FILE.798875579" name="Specify output file name (--output_file, -o)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.OUTPUT_FILE" value="&quot;${ProjName}.out&quot;" valueType="string"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.MAP_FILE.658950961" name="Input and output sections listed into &lt;file&gt; (--map_file, -m)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.MAP_FILE" value="&quot;${ProjName}.map&quot;" valueType="string"/>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.SEARCH_PATH.340263356" name="Add &lt;dir&gt; to library search path (--search_path, -i)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.SEARCH_PATH" valueType="stringList">
    									<listOptionValue builtIn="false" value="&quot;${CG_TOOL_ROOT}/lib&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;${CG_TOOL_ROOT}/include&quot;"/>
    								</option>
    								<option id="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.LIBRARY.444212762" name="Include library file or command file as input (--library, -l)" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.linkerID.LIBRARY" valueType="libs">
    									<listOptionValue builtIn="false" value="&quot;libc.a&quot;"/>
    								</option>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exeLinker.inputType__CMD_SRCS.640571522" name="Linker Command Files" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exeLinker.inputType__CMD_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exeLinker.inputType__CMD2_SRCS.1130196640" name="Linker Command Files" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exeLinker.inputType__CMD2_SRCS"/>
    								<inputType id="com.ti.ccstudio.buildDefinitions.C6000_7.3.exeLinker.inputType__GEN_CMDS.2110630641" name="Generated Linker Command Files" superClass="com.ti.ccstudio.buildDefinitions.C6000_7.3.exeLinker.inputType__GEN_CMDS"/>
    							</tool>
    							<tool id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.226238413" name="XDCtools" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool">
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.XDC_PATH.44416606" name="Package repositories (--xdcpath)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.XDC_PATH" valueType="stringList">
    									<listOptionValue builtIn="false" value="&quot;${BIOS_CG_ROOT}/packages&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;${BIOSPSP_INSTALL_DIR}/drivers&quot;"/>
    									<listOptionValue builtIn="false" value="&quot;C:\Licor\li6840DSP\dspsrc&quot;"/>
    									<listOptionValue builtIn="false" value="${TARGET_CONTENT_BASE}"/>
    								</option>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.TARGET.359508193" name="Target (-t)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.TARGET" value="ti.targets.C674" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM.1703141961" name="Platform (-p)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM" value="L138SOM" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM_RAW.1257005979" name="Platform (-p)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.PLATFORM_RAW" value="L138SOM" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_PROFILE.1109575038" name="Build-profile (-r)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_PROFILE" value="release" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_CONFIGURATION_FILE.1173860905" name="Build configuration file (-b)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.BUILD_CONFIGURATION_FILE" value="&quot;${PROJECT_ROOT}/L138SOM/config.bld&quot;" valueType="string"/>
    								<option id="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.CODEGEN_TOOL_DIR.1831695366" name="Compiler tools directory (-c)" superClass="com.ti.rtsc.buildDefinitions.XDC_3.16.tool.CODEGEN_TOOL_DIR" value="&quot;${CG_TOOL_ROOT}&quot;" valueType="string"/>
    							</tool>
    						</toolChain>
    					</folderInfo>
    					<fileInfo id="com.ti.ccstudio.buildDefinitions.C6000.Release.1799793832.OMAPL138_DSP.gel" name="OMAPL138_DSP.gel" rcbsApplicability="disable" resourcePath="OMAPL138_DSP.gel" toolsToInvoke=""/>
    					<sourceEntries>
    						<entry excluding="OMAPL138_DSP.gel|L138SOM/package/build.cfg" flags="VALUE_WORKSPACE_PATH|RESOLVED" kind="sourcePath" name=""/>
    					</sourceEntries>
    				</configuration>
    			</storageModule>
    			<storageModule moduleId="org.eclipse.cdt.core.externalSettings"/>
    		</cconfiguration>
    	</storageModule>
    	<storageModule moduleId="cdtBuildSystem" version="4.0.0">
    		<project id="li6840.com.ti.ccstudio.buildDefinitions.C6000.ProjectType.266474454" name="C6000" projectType="com.ti.ccstudio.buildDefinitions.C6000.ProjectType"/>
    	</storageModule>
    	<storageModule moduleId="refreshScope" versionNumber="1">
    		<resource resourceType="PROJECT" workspacePath="/li6840"/>
    	</storageModule>
    	<storageModule moduleId="org.eclipse.cdt.core.language.mapping">
    		<project-mappings>
    			<content-type-mapping configuration="" content-type="org.eclipse.cdt.core.asmSource" language="com.ti.ccstudio.core.TIASMLanguage"/>
    			<content-type-mapping configuration="" content-type="org.eclipse.cdt.core.cHeader" language="com.ti.ccstudio.core.TIGCCLanguage"/>
    			<content-type-mapping configuration="" content-type="org.eclipse.cdt.core.cSource" language="com.ti.ccstudio.core.TIGCCLanguage"/>
    			<content-type-mapping configuration="" content-type="org.eclipse.cdt.core.cxxHeader" language="com.ti.ccstudio.core.TIGPPLanguage"/>
    			<content-type-mapping configuration="" content-type="org.eclipse.cdt.core.cxxSource" language="com.ti.ccstudio.core.TIGPPLanguage"/>
    		</project-mappings>
    	</storageModule>
    	<storageModule moduleId="org.eclipse.cdt.internal.ui.text.commentOwnerProjectMappings"/>
    	<storageModule moduleId="scannerConfiguration"/>
    	<storageModule moduleId="org.eclipse.cdt.core.LanguageSettingsProviders"/>
    </cproject>
    

  • I'm posting my project file which now doesn't work even after reverting to v5.3 that uses 7.4.1 compiler. CCSv5.3 has the same problem whenever I change in project settings the compiler version from 7.3.11 to 7.4.1. I cannot compile the code anymore, deleting ti folder didn't help. Now I'm completely stuck.6012.ccs.zip

  • I am running into this same issue on a Hercules project.

  • Hi,

    I get the same error with our projects in CCS v5.4 when switching CG Tools Versions, e.g. from 7.3.8 to 7.4.2, or 7.2.7 to 7.3.8. It happens with C64x and C64+ Projects, I didn't observe this with my C66x projects.

    Ralf

  • Hello,

    I also got some logs when running from command line, hope this is helpful. This time the projects have been created from scratch in CCSv5.4.

    org.eclipse.core.internal.resources.ResourceException: Errors occurred during the build.
    at org.eclipse.core.internal.resources.Workspace.buildInternal(Workspace.java:525)
    at org.eclipse.core.internal.resources.Workspace.build(Workspace.java:432)
    at com.ti.ccstudio.project.core.services.ProjectBuilder.internalBuildProjects(ProjectBuilder.java:242)
    at com.ti.ccstudio.project.core.services.ProjectBuilder.buildProjects(ProjectBuilder.java:176)
    at com.ti.ccstudio.project.core.services.ProjectBuilder.buildProjects(ProjectBuilder.java:165)
    at com.ti.ccstudio.apps.internal.project.Build.buildProjects(Build.java:252)
    at com.ti.ccstudio.apps.internal.project.Build.doRun(Build.java:108)
    at com.ti.ccstudio.apps.internal.BaseHeadlessApp$2.run(BaseHeadlessApp.java:264)
    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2344)
    at com.ti.ccstudio.apps.internal.BaseHeadlessApp.internalRun(BaseHeadlessApp.java:262)
    at com.ti.ccstudio.apps.internal.BaseHeadlessApp.start(BaseHeadlessApp.java:216)
    at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)
    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:110)
    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:79)
    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:353)
    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:180)
    at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
    at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
    at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
    at java.lang.reflect.Method.invoke(Unknown Source)
    at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:629)
    at org.eclipse.equinox.launcher.Main.basicRun(Main.java:584)
    at org.eclipse.equinox.launcher.Main.run(Main.java:1438)
    Contains: Errors running builder 'CDT Builder' on project 'UnitTest'.
    java.lang.NullPointerException
    at org.eclipse.cdt.managedbuilder.internal.core.Tool.getOutputExtension(Tool.java:2355)
    at com.ti.ccstudio.project.core.internal.build.temp.GnuMakefileGenerator.addRuleForSource(GnuMakefileGenerator.java:2125)
    at com.ti.ccstudio.project.core.internal.build.CCSMakefileGenerator.addRuleForSource(CCSMakefileGenerator.java:925)
    at com.ti.ccstudio.project.core.internal.build.temp.GnuMakefileGenerator.addFragmentMakefileEntriesForSource(GnuMakefileGenerator.java:1857)
    at com.ti.ccstudio.project.core.internal.build.CCSMakefileGenerator.addFragmentMakefileEntriesForSource(CCSMakefileGenerator.java:813)
    at com.ti.ccstudio.project.core.internal.build.temp.GnuMakefileGenerator.addSources(GnuMakefileGenerator.java:1762)
    at com.ti.ccstudio.project.core.internal.build.temp.GnuMakefileGenerator.populateFragmentMakefile(GnuMakefileGenerator.java:617)
    at com.ti.ccstudio.project.core.internal.build.temp.GnuMakefileGenerator.regenerateMakefiles(GnuMakefileGenerator.java:570)
    at com.ti.ccstudio.project.core.internal.build.CCSMakefileGenerator.regenerateMakefiles(CCSMakefileGenerator.java:358)
    at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performMakefileGeneration(CommonBuilder.java:1006)
    at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.performPrebuildGeneration(CommonBuilder.java:873)
    at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:748)
    at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:513)
    at org.eclipse.cdt.managedbuilder.internal.core.CommonBuilder.build(CommonBuilder.java:459)
    at org.eclipse.core.internal.events.BuildManager$2.run(BuildManager.java:728)
    at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:42)
    at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:199)
    at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:239)
    at org.eclipse.core.internal.events.BuildManager$1.run(BuildManager.java:292)
    at org.eclipse.core.runtime.SafeRunner.run(SafeRunner.java:42)
    at org.eclipse.core.internal.events.BuildManager.basicBuild(BuildManager.java:295)
    at org.eclipse.core.internal.events.BuildManager.basicBuildLoop(BuildManager.java:351)
    at org.eclipse.core.internal.events.BuildManager.build(BuildManager.java:374)
    at org.eclipse.core.internal.resources.Workspace.buildInternal(Workspace.java:513)
    at org.eclipse.core.internal.resources.Workspace.build(Workspace.java:432)
    at com.ti.ccstudio.project.core.services.ProjectBuilder.internalBuildProjects(ProjectBuilder.java:242)
    at com.ti.ccstudio.project.core.services.ProjectBuilder.buildProjects(ProjectBuilder.java:176)
    at com.ti.ccstudio.project.core.services.ProjectBuilder.buildProjects(ProjectBuilder.java:165)
    at com.ti.ccstudio.apps.internal.project.Build.buildProjects(Build.java:252)
    at com.ti.ccstudio.apps.internal.project.Build.doRun(Build.java:108)
    at com.ti.ccstudio.apps.internal.BaseHeadlessApp$2.run(BaseHeadlessApp.java:264)
    at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2344)
    at com.ti.ccstudio.apps.internal.BaseHeadlessApp.internalRun(BaseHeadlessApp.java:262)
    at com.ti.ccstudio.apps.internal.BaseHeadlessApp.start(BaseHeadlessApp.java:216)
    at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:196)
    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:110)
    at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:79)
    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:353)
    at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:180)
    at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
    at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
    at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
    at java.lang.reflect.Method.invoke(Unknown Source)
    at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:629)
    at org.eclipse.equinox.launcher.Main.basicRun(Main.java:584)
    at org.eclipse.equinox.launcher.Main.run(Main.java:1438)

    Best regards,

    David.

  • I also have this problem with a C66xx project now.
    Is there any progress on this issue?

    Thanks,
    Ralf

  • Hello,

    We believe this issue is the same as another reported issue:

    http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/275061.aspx

    The fix for this issue will be in the CCSv5.5 release coming in September.

    For more details on the issue, and a workaround, see the last post in the above mentioned thread.

    Thanks

    ki