Other Parts Discussed in Thread: CONTROLSUITE
Good Morning,
I am resending this post because the answer I got the last time handled a CMD file issue and actually didn't answer the base question posed below. I am working with several people now and this issue keeps coming up. There must be a way to force all the underlying C source files to be transferred into the workspace locally, so that changes to them will not ruin the files in the ControlSuite directories. The only thing I have been able to accomplish at this point is to individually bring in source files in using manual copies, which is very tedious. Has anyone been able to get by this problem? See the following question description of the problem.
I have imported about 15 different projects over the past several weeks and have worked with and modified them to learn how to use the peripherals on my M36 Concerto part. I found out that the imports do not actually copy the files to my workspace, but link to the original ControlSuite directories. As a result I don't have any of the original projects in untouched form! I did the copy all option when I did the Imports, but I am positive the files aren't copied because I tested it this morning. I will now have to reload controlsuite files somewhere to get the original files back. However I can't put them in the default location because it will destroy all the work I have done these past weeks.
I need to know how to put ALL the project files into my new workspace so I don't have any links to the ControlSuite copies I referenced. I have looked through the documentation and have not been able to find a way to do it. Does anyone know how I can get all the project files in the workspace with no files having the linked file property?
Sincerely,
Mike Fontes