Hi,
I have a question about CCSv5.
I'm having a problem with Memory Browser.
After launching Debugger and connect to the target,
when I enter address(0x80000000) to Memory Browser the following message appears:
********************************************************************************
CortxA8: Trouble Reading Memory Block at 0x80000000 on Page 0 of Length 0x228:
(Error -2030 @ 0xF) Internal error: Access to unknown or invalid register was requested.
Restart the application. If error persists, please report the error. (Emulation package 5.0.857.0)
********************************************************************************
I thought it was DDR2 configuration problem but it also occurs
when entering other area address to Memory Browser, for example 0x402F0400(Internal Shared Memory).
So, it's not DDR2 configuration problem.
What is the cause of this error?
And are there any workaround for this error?
By the way, I'm using CCSv5.2.1 and conneting AM3358EVM.
best regards,
g.f.