This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code Composer displays error: errors occurred while reading C:\\Users\\brentw\\AppData\\Local\\Temp\\042728

I am using Code Composer Version 4.2.1.0004.

I am importing an existing project.

When I attempt to build I get the following error after each source file that is being built:

error: errors occurred while reading   

    C:\\Users\\brentw\\AppData\\Local\\Temp\\042728

NOTE:  The temp folder created is different for each file that is being built.

Any help would be appreciated.

Thanks,

Brent