Other Parts Discussed in Thread: TMS320C6414T
Hi,
I'm comming from CCS3.3 with a Project (C6414) giving simple "Status Messages" via LOG_printf to the CCS3.3.
(Not really live, but displayed with a reasonable delay in the "trace" window).
I converted the Project to CCS5 (5.3.0.00090, now using DSP/BIOS 5.42.0.07). As the LOG_printf - Outputs do not occur i searched this Forum:
http://e2e.ti.com/support/embedded/bios/f/355/t/238859.aspx
It finally tells that I should go for RTDX
("DSP/BIOS supports stopmode (which you've used). To get the data off without halting the processor, you can try to use RTDX. However, TI no longer officially supports this interface.")
But I was not able to "activate" RTDX to achieve what I wanted.
http://e2e.ti.com/support/embedded/bios/f/355/t/221397.aspx
http://e2e.ti.com/support/embedded/bios/f/355/p/193476/692775.aspx#692775
Tell that CCS5 does not Support RTDX.
1.) Is it correct that there is no possibility to get a printf-output while the DSP is running (CCS5/DSP-BIOS) ?
Hence I wanted to do this with "System Analyzer" and found (spruh43d.pdf) that it requires SYS/BIOS.
Hence I wanted to Switch to SYS/BIOS and found (spraas7g.pdf) that
"SYS/BIOS 6 does not support all targets that were previously supported by DSP/BIOS 5. The
following targets are not supported by SYS/BIOS 6: C54x, C55x, C62x, C64x, and C67x."
2.) Hence is it correct that there is no way to get Feedback from the DSP while it is running in my case (TMS320C6414T) ?
Excuse that I ask this but I just can't believe my conclusion.
Regards, Wolfgang