This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We recently installed CCS5.2 on new PC with windows 7 ... we get the following. erros msgs (see attached )
I have tried to set Xls and Xmx to correct but it doesnt help .. here's what i've done:
Ccstudio.ini
-startup
plugins/org.eclipse.equinox.launcher_1.2.0.v20110502.jar
-product
com.ti.ccstudio.branding.product
--launcher.XXMaxPermSize
256M
-showsplash
com.ti.ccstudio.branding
--launcher.defaultAction
openFile
-vmargs
-Dosgi.requiredJavaVersion=1.5
-Dosgi.instance.area.default=@user.home/workspace_v5_2
-Xms128m
-Xmx512m
-XX:ErrorFile=C:\Users\e709628\AppData\Local\.TI\213602635\0\dmp\hs_err_%p.log
Eclipse.ini
-startup
plugins/org.eclipse.equinox.launcher_1.2.0.v20110502.jar
--launcher.library
plugins/org.eclipse.equinox.launcher.win32.win32.x86_1.1.100.v20110502
-product
org.eclipse.epp.package.cpp.product
--launcher.defaultAction
openFile
--launcher.XXMaxPermSize
256M
-showsplash
org.eclipse.platform
--launcher.XXMaxPermSize
256m
--launcher.defaultAction
openFile
-vmargs
-Dosgi.requiredJavaVersion=1.5
-Xms128m
-Xmx512m
I even tried this .. (See attachement)
Here is my PC configuration (see attachement)
Any help woul dbe appreciated.
We have fixed the issue .. I figured out how to display the heap status. I crept up to the mark and back down. and now it works ... no need to further investigate .. thanks ..
Hi Rick,
that is great to hear and thanks for the update.
All the best with development.
Best regards,
Lisa