Other Parts Discussed in Thread: CCSTUDIO
Hi
I imported my ccsv3.3 .pjt file and have the errors below.
I checked the directory and the .cfg and .dat file are present.
And then I noticed that my .tcf file is "excluded from the build" according the the eclipse project viewer.
I found this in the Wiki
"If you have a DVSDK project that has both a .tcf (DSP/BIOS configuration) and a .cfg (RTSC configuration for drivers...) the import tool in beta 2 will not allow you to import this project. There are complications with using both forms of configuration in a project so the import tool will prevent this for now."
Do I have to change my ccsv3.3 to not use a .cfg file so that I can import into ccsv4.1?
Maybe I should give up on the import tool and create a new clean project from scratch?
Cheers
********* ************* *********** ************* *******************
Directory of C:\Work\CloudCap\DSP\TASE_VPS_LT_DSP\VPS-CCsv4\config
12/20/2009 01:06 PM <DIR> .
12/20/2009 01:06 PM <DIR> ..
12/20/2009 12:54 PM 579 dm648_uart0.tci
12/20/2009 12:54 PM 596 dm648_vport0.tci
12/20/2009 12:54 PM 596 dm648_vport1.tci
12/20/2009 12:54 PM 596 dm648_vport2.tci
12/20/2009 12:54 PM 596 dm648_vport3.tci
12/20/2009 12:54 PM 596 dm648_vport4.tci
12/20/2009 01:06 PM <DIR> obj
12/20/2009 12:54 PM 156,089 TASE_LT_DM648.gel
12/20/2009 12:54 PM 778 tase_lt_vps.cfg
12/20/2009 12:54 PM 6,188 tase_lt_vps.tcf
12/20/2009 01:04 PM 410 tase_lt_vps.tco
12/20/2009 01:07 PM <DIR> xdcconfig
12/20/2009 12:54 PM 334 xdcpaths.dat
11 File(s) 167,358 bytes
4 Dir(s) 206,759,481,344 bytes free
*************migration.log file****************************************************************************8
!ERROR: Unresolved source file: config/tase_lt_vps.cfg
!ERROR: Unresolved source file: config/xdcpaths.dat
!WARNING: Unresolved tool: com.ti.ccstudio.buildDefinitions.C6000.Debug.1978214633::XDC
!CONFIGURATION: 'com.ti.ccstudio.buildDefinitions.C6000.Debug.1978214633' [Sun Dec 20 13:24:18 PST 2009]
!TOOL: 'com.ti.rtsc.buildDefinitions.DSPBIOS_5.40.tool.1944753017./tase_lt_vps/config/tase_lt_vps.tcf'
!WARNING: Unresolved option: com.ti.rtsc.buildDefinitions.DSPBIOS_5.40.tool.1944753017./tase_lt_vps/config/tase_lt_vps.tcf::-v6x
!WARNING: Unresolved tool: com.ti.ccstudio.buildDefinitions.C6000.Default.1739920003::XDC
!CONFIGURATION: 'com.ti.ccstudio.buildDefinitions.C6000.Default.1739920003' [Sun Dec 20 13:24:28 PST 2009]
!TOOL: 'com.ti.rtsc.buildDefinitions.DSPBIOS_5.40.tool.1329958297./tase_lt_vps/config/tase_lt_vps.tcf'
!WARNING: Unresolved option: com.ti.rtsc.buildDefinitions.DSPBIOS_5.40.tool.1329958297./tase_lt_vps/config/tase_lt_vps.tcf::-v6x
!WARNING: Unresolved tool: com.ti.ccstudio.buildDefinitions.C6000.Default.534338649::XDC
!CONFIGURATION: 'com.ti.ccstudio.buildDefinitions.C6000.Default.534338649' [Sun Dec 20 13:24:29 PST 2009]
!TOOL: 'com.ti.rtsc.buildDefinitions.DSPBIOS_5.40.tool.27526656./tase_lt_vps/config/tase_lt_vps.tcf'
!WARNING: Unresolved option: com.ti.rtsc.buildDefinitions.DSPBIOS_5.40.tool.27526656./tase_lt_vps/config/tase_lt_vps.tcf::-v6x
!WARNING: Unresolved tool: com.ti.ccstudio.buildDefinitions.C6000.Release.1142514620::XDC
!CONFIGURATION: 'com.ti.ccstudio.buildDefinitions.C6000.Release.1142514620' [Sun Dec 20 13:24:29 PST 2009]
!TOOL: 'com.ti.rtsc.buildDefinitions.DSPBIOS_5.40.tool.626458904./tase_lt_vps/config/tase_lt_vps.tcf'
!WARNING: Unresolved option: com.ti.rtsc.buildDefinitions.DSPBIOS_5.40.tool.626458904./tase_lt_vps/config/tase_lt_vps.tcf::-v6x