This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

System analyser/hardware trace missing in Perspective based on CCS Debug



Hello,

(target C6678, CCS 5.5)

I'm creating a personnalised Perspective based on CCS Debug.

However in the Tools menu : Hardware trace and System Analyser are missing.

In CCS Debug they are present.

I think it's a bug.
You can reproduce it easily :
On a new workspace, open the CCS debug perspective. Right click "save as" MyDebug.
In CCS debug : tools -> Hardware trace and System Analyser are available
In MyDebug : tools -> Hardware trace and System Analyser are missing

Regards,
Clement