Hi everybody!
I am experiencing currently an erratic behavior of CCSv4/Eclipse. I installed the test projects that were included on the eZdsp USB stick installation CD (i.e. led, spirom and aic3204). I am able to install these projects correctly, compile them and run them.
Sometimes, when I start CCS and try to rebuild any of these projects, the following error message pops up:
This project was created for a device-variant that is not currently recognized TMS320C55XX.TMS320C5505. Please install the device-variant descriptor, or migrate the project to one of the supported device-variants.
That is strange because of two things: First, I was able to build the project before, and second, because the device-variant descriptor (under Project properties-->CCS build settings-->Project settings) has changed. While it indicated "TMS320C5505" before when everthing was fine, it now shows "TMS320C55XX.TMS320C5505". Furthermore, when I click on "more" to select the correct device variant (TMS320C5505), it only shows three device variants (something like Custom C5505, Standard C5505 and something else) but not TMS320C5505 or any of the other, usually available options.
Has anyone else experienced this behavior and knows how to fix it? I usually restart CCS again and sometimes that helps, but that is a bit unsatisfactory, especially since it only helps sometimes.
Cheers and thanks in advance!