This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issues after updating CCS from 4.2.1 to 4.2.4



Hi,

 

I just updated CCS from v4.2.1 to v4.2.4. Also, updated to latest CGT, Spectrum Digital updates, etc.

I initiated the update through Help-->Software-->Find and Install

After the update was finished I couldn't build any of the existing projects. I got the following message:

"This project was created for a device-variant that is not currently recognized: TMS320C55XX.TMS320VC5515. Please install the device-variant descriptor, or migrate the project to one of the supported device-variants. "

When I tried to go into  CCS Build in Project Properties I got the following message: "The currently displayed page contains invalid values".

 

Any idea how to solve this without a complete uninstall of CCS (I don't want to have to separately download the full image of CCS 4.2.4 or downgrade to a version that clearly has problems) ?

 

Thanks,

Shahar