This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have some ARM A15 code built with CCS 5.5/BIOS/XDC, running on K2H EVM. When load the code and run using CCS 5.4, there is no problem to halt the ARM core, read memory, check expression window and so on. However, when load and run the same code using CCS 5.5, I sometimes can't halt the ARM core (JTAG failure).
Regards, Eric
This issue was resolved offline. The issue was with a known bug in the debug server that comes with CCSv5.5. Updating the debug server will resolve the issue. To do this:
Thanks
ki