Hi all! I'm getting started with a project on the MSP430FR5739, and I'm getting an unfamiliar compiler warning. The warning shows that this issue is coming from the header file of my microcontroller (msp430fr5739.h). This is the compiler warning:
#10083-D LOAD placement ignored for "SIGNATURE_MEMORY": object is uninitialized
Even though the warning comes from outside my code, I've posted a simplified version of my code below.
#include <msp430.h> #include <stdio.h> #include <stdlib.h> #include <stdbool.h> /* * main.c */ int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer /*************CLOCK INITIALIZER*************/ //Writes password to enable CS register access CSCTL0_H = 0xA5; //Set max. DCO setting to 24MHz CSCTL1 |= DCOFSEL0 + DCOFSEL1 + DCORSEL; // Sets the MCLK source to DCOCLK, // the SMCLK source to DCOCLK, // and the ACLK source to VLOCLK CSCTL2 = SELM0 + SELM1 + SELS0 + SELS1 + SELA0; // Sets the MCLK clock divider to 0, // the SMCLK clock divider to 0, // and the ACLK clock divider to 0, CSCTL3 &= 0x00; // Enables conditional module requests for // MCLK, SMCLK, and ACLK CSCTL6 |= MCLKREQEN + SMCLKREQEN + ACLKREQEN; /*************TEMPRETURE SENSOR CONTROL*************/ // Turn off temp sensor REFCTL0 |= REFTCOFF; REFCTL0 &= ~REFON; /*************CONFIGURE MPU*************/ MPUCTL0 = MPUPW; // Write PWD to access MPU registers //Add any changes to the MPU here MPUSEG = 0x0804; // B1 = 0xC800; B2 = 0xD000 // Borders are assigned to segments MPUCTL0 = MPUPW+MPUENA; // Enable MPU protection return 0; } // trap ISR assignment - put all unused ISR vector here #pragma vector = PORT1_VECTOR, ADC10_VECTOR, PORT2_VECTOR, \ TIMER0_A0_VECTOR, TIMER0_A1_VECTOR, WDT_VECTOR, COMP_D_VECTOR, \ DMA_VECTOR, PORT3_VECTOR, PORT4_VECTOR, RTC_VECTOR, \ SYSNMI_VECTOR, TIMER0_B0_VECTOR, TIMER0_B1_VECTOR, \ TIMER1_A0_VECTOR, TIMER1_A1_VECTOR, TIMER1_B0_VECTOR, \ TIMER1_B1_VECTOR, TIMER2_B0_VECTOR, TIMER2_B1_VECTOR, \ UNMI_VECTOR, USCI_A1_VECTOR, USCI_B0_VECTOR, USCI_A0_VECTOR __interrupt void TrapIsr(void) { // this is a trap ISR - check for the interrupt cause here by // checking the interrupt flags, if necessary also clear the interrupt // flag }
The good news is that it doesn't seem to cause any issues when I'm actually running the code (even when I add simple toggle-pin functions). However, I would like to know what this compiler warning actually means and, if possible, fix this issue. Any suggestions?