Other Parts Discussed in Thread: CCSTUDIO
I saw the official release announcement for CCS 4.1, but it isn't very clear what the availability of it and especially any related files are in terms of updated download locations.
As for CCStudio itself, the only download page that I'm aware of for the full image release which was said to be available in the 4.1 release announcement is here:
http://focus.ti.com/docs/toolsw/folders/print/ccstudio.html
http://software-dl-1.ti.com/dsps/forms/self_cert_export.html?prod_no=setup_CCS_4_Platinum.zip&ref_url=http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/CCSv4/latest/
But nothing on the page or link indicates whether it is 4.1, it only says 4.1, and "latest". So I'm hoping that all the links for MCU / Platinum are updated on the download site.
In fact the ccstudio page itself is not reassuring about the updates having been made, since Stellaris support is explicitly disclaimed whereas that is a main feature of CCS 4.1,
so that leads to more doubts about whether that is the right download page (also it doesn't claim support for Windows 7 which I thought CCS 4.1 also brought):
Product versions
- There are 2 versions of CCS, Platinum and Microcontroller. They differ in the processors they support.
- Cores Supported
- Platinum Edition: TMS320C6000, TMS320C5000, TMS320C2800, TMS470, TMS570, ARM 7, ARM9, ARM 11, ARM Cortex M3 (Not including Stellaris Cortex M3), ARM Cortex R4, ARM Cortex A8, and MSP430
- Microcontroller Edition: TMS320C2800 and MSP430
- Both CCS Platinum and Microcontroller use the following:
- Host: PC
- OS: Microsoft Windows Vista and XP
- Cores Supported
Stellarisware upades for ccs 4.1:
On the 4.1 beta page, for instance, there was an explicit list of several StellarisWare packages related to the 4.1 Beta, I assume these may also have been
new versions of the Stellaris files specifically to interoperate with CCS 4.1 Beta. Are the corresponding new Stellaris files now also officially released / updated for
use with CCS 4.1, and if so, are the download links for all the Stellaris components on the regular TI web pages going to now refer to the new versions?
For instance if you look at the Stellaris related web pages you sometimes do not see any explicit version information corresponding to the version available for download
as is the case here, so one is left to wonder if the linked versions are new for CCS 4.1 or not at this time:
http://focus.ti.com/docs/toolsw/folders/print/sw-lm3s.html
On the "Stellaris Software updates" page the most recent file dates are October 2009 which leads me to think that either this page has not yet been updated or
that the files themselves may not need official updates at this time (in which case I wonder what was different if anything about the StellarisWare for CCS 4.1 Beta files
listed on the CCS 4.1 Beta wiki page):
http://focus.ti.com/mcu/docs/mcuorphan.tsp?contentId=87903
versus
http://tiexpressdsp.com/index.php/Beta_Releases_CCS
StellarisWare (for CCSv4.1 Beta)
Documentation
Firmware Development Packages
- EK-LM3S811-5451
- EK-LM3S1968-5451
- EK-LM3S2965-5451
- EK-LM3S3748-5451
- EK-LM3S6965-5451
- EK-LM3S8962-5451
- EK-LM3S9B90-5451
- EK-LM3S9B92-5451
- SW-RDK-IDM-5451
- SW-RDK-IDM-L35-5451
- SW-RDK-IDM-SBC-5451
- SW-RDK-S2E-5451
- SW-RDK-ACIM-5451
- SW-RDK-BDC-5451
- SW-RDK-BLDC-5451
- SW-RDK-STEPPER-5451
- SW-DK-LM3S9B96-5451
Miscellaneous
- RDK-ACIM GUI Installer
- RDK-BLDC GUI Installer
- RDK-STEPPER GUI Installer
- RDK-S2E Windows configuration utility
- Windows-side examples for USB kits
- Luminary Micro embedded USB drivers