This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to use fgetc using code composer. After opening a .csv file using fopen, I try to get the characters in the file via fgetc. However, the file pointer points to EOF by default when I go into the do-while loop into the checklen function below. We tried to exact same code on MS Visual Studio and it works fine on there. Here's a snippet of the relevant code:
arrayprop chartoint(char * input, char * mode){
int length=0; //for length of char array
FILE *file;
file=fopen(input, mode); //The location of the txt file. Note the FORWARD slash. In read-only mode
length=checklen(file); //Find the length of the file so enough memory can be allocated
}
The program finds the file but messes up in checklen(file) when I try to find the number of chars within the file
int checklen(FILE *pfile){//Checks how many chars there are in the csv file
int c=0; //just so the fgetc function has somewhere to return values to, though fgetc returns them as chars
int length=0; //this is what this function will return at the end
do{
c=fgetc(pfile); //just use the fgetc function and pass in the file pointer. pfile is incremented implicitly
length++; //increment the length counter for every char (byte) found
} while(c!=EOF);//do this until the end of file, at which point length will be the size of the file
return length; //return the size of the file
}
c gets -1 on its first pass in the do-while loop, which means the file pointer is pointing to EOF by default. Why is this happening and what can I do to fix it?
Make sure you are not running out of stack or heap. Check other tips like this in this wiki article.
Thanks and regards,
-George
Are you using a target with 16-bit "char"?
Are you trying to read a non-ASCII file?